Part Number: LM75A Hello E2E,
Our customer is trying the LM75 with there test board. When they written 0x3C00 to Thyst register, the device output 0x3CFF when read. Is it malfunction? Or is there a problem with how to use it?
Best regards, ACGUY
Part Number: LM75A Hello.
We consider to use this PN for space low orbit application. Please let me know if you have performed any radiation screening on these parts.
Thank you in advance, Michael
Part Number: LM75A
Hi,
In LM75A datasheet, t conversion time is mentioned as 100ms to 300ms with a note that specifies that LM75A should not be accessed continuously with a wait time of less than 300ms. As if it happens, the conversion that in progress…
Part Number: LM75A Other Parts Discussed in Thread: LM70 , LM75B , LM73 Hi Sir,
May I know the heat flow used on LM75A which pin-out?
Temperature sensors: PCB guide lines for surface mount devices: https://www.ti.com/lit/an/snoa967a/snoa967a.pdf
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: LM75A , AM3352 , SYSCONFIG
Hi,
We are using LM75A temperature sensor to measure the temperature value of our custom board.
LM75A Temperature is directly connected to am3352 I2C0 bus using…
Part Number: LM75A Other Parts Discussed in Thread: TMP117 , TMP116 Hi Team,
There is a question of LM75A. In the datasheet, recommended operating conditions of TJ temp range is -55C~125C.
What's the absolute maximum ratings of Tj Max? Can we support…
Part Number: LM75A Other Parts Discussed in Thread: TMP1075 Hi Team,
The datasheet of LM75A mentioned the Configuration Register of D5~D7 as below:
D5–D7: These bits are used for production testing and must be kept zero for normal operation.
My…
Part Number: LM75SW-LINUX Tool/software: TI C/C++ Compiler Our core chip is Amlogic T972,
and we use this file to build the driver, but we can't compile success,
there lost some definition in head file,
please help provide some solution for us, thanks…
Part Number: LM75A Other Parts Discussed in Thread: ADC128D818 Q1:I2C interface electrical characteristic, What is the maximum allowable rise time?
Q2:If SDA and SCL rise time is 3.2usec, is there a problem happen?(SCL frequency is 25kHz)
Is there any…
Part Number: LM75A Other Parts Discussed in Thread: LM75B , , TMP1075 HI Team,
I have some questions about LM75, could you help to reply these questions below.
Customer use LM75BD (NXP) solutions, we try to propose our solutions to them.
The project timescale…