Part Number: LM76002 Hello,
my Customer would like to know this device available to use their condition below.
VIN: 18-36V
VOUT: 12-16V
IOUT: 1.5A
Webebnch shows us simulation result of 73.13 deg of phase margin with Fsw=500kHz. In this situation, switching…
Part Number: LM76002 All,
Customer would like to use the output of the LM76002 (Vin= 24V) in an Oring configuration with 48V source. When the 48V is present the LM76002 will see 48V on the output and will turn off. Two questions.
Can the LM76002 withstand…
Part Number: LM76002-Q1 Hello,
we are using the LM76002-Q1 in an automotive USB charger.
Has a reference design with this device been tested according to ISO7637-2 by TI? Does a reverse polarity protection diode suffice to reach ISO Pulse immunity Level…
Part Number: LM76002 Hello,
I want to purchase LM76002RNPR but is not available in mouser, digikey lead time is 6 weeks.
In those websites LM76002RNPT is available, Can you tell me what is difference between these two?
Can i purchase LM76002RNPT instead…
Part Number: LM76002 Hi
Pluese let me ask you about inductor of LM76002.
My customer will use LM76002 the following condition.
But they will use NS12575T330MN as inductor because it is cheaper than the inductor of 10uF.
Can they use this inductor with…
Part Number: LM76002 Other Parts Discussed in Thread: LM43602 hello,
from the block diagram in the datasheet there is difference below between LM43602 and LM76002. could you tell me what the real difference between them?
1. in the 43602 the PFM detector…
Part Number: LM76002 Hi
I got a question from my customer about LM76002.
I think there are delay time by being PG high after rised Vout.
Are there those specified value?
Best regards,
Yokota
Part Number: LM76002 On LM76002EVM, MODE pin is connected to VCC for FPWM operation.
Is this connection no problem although there is comment "TI does not recommended loading this pin by external circuitry." on datasheet?
Can we connect MODE…
hi, Jim,
I have below ,please check it it works. LM76002-Q1 , LMR14020-Q1
The OCP is not adjustable for this convertor, do you prefer with FET inside IC or outside.
Elena
Part Number: LM76002-Q1 Hello Team, please could you explain following values in the table which we cannot find in the datasheet description
Means this that part will be disabled by EN-Voltage lower than 0.3V and Enable higher than 1.2V?
Many Thanks …