Part Number: AWR1843AOP Other Parts Discussed in Thread: AWR2944EVM , LM76003 , LM63635-Q1 Tool/software: When I use the AWR1843AOP considering truck/bus radar, the power supply must be configured to a maximum input of 29V typical and 60V transient.
Therefore…
Part Number: LM76003 Hello team,
Is there any difference between LM76003 and LM76003-Q1 besides Q1 rating and the CDM ESD rating? Customer is looking to swap between the parts based on availability, so wanted to make sure we're not missing anything. …
Part Number: LM76003-Q1 hi,
i am referring to the same question here: (12) LM76003-Q1: Hot issue on LM76003-Q1 - Power management forum - Power management - TI E2E support forums
Now i have another board having all the three LM76003-Q1 b urn out as shown…
Part Number: LM76003-Q1 Hello,
I am designing a dc-dc converter with part LM76003QRNPRQ1 and after reviewing datasheet and simulator results I do not understand well input capacitors selection criteria.
According to the datasheet it is required a input…
Part Number: LM76003-Q1 Dear Sir/ Madam,
We are using 3 of the LM76003-Q1 to supply the power to MCU and peripheral. Now we faced the ot issue, Here i attached the circuit diagram.
1. Vin range =46-50V 2. Vout = 24V 3. Iout nominal =0.3A 4. Ambient temp…
Part Number: LM76003-Q1 Other Parts Discussed in Thread: LM76003 Dear Sir,
Does lm76003 need input reverse polarity protection?
---------------------------------------------------------------------------
System power supply: 24VDC battery
ECU function…
Part Number: LM76003-Q1 Other Parts Discussed in Thread: LM5141 , LM61440 Hi,
is it possible to introduce the "spread spectrum" on the dc / dc LM76003-Q1? Or is there a version that contemplates it? Thanks so much,
Antonio
Part Number: LM76003-Q1 Other Parts Discussed in Thread: LM76002-Q1 , , LM5576 May I know does the Does the LM76003-Q1 and LM76002-Q1 pass ISO7637 test? Could you share the test report?
We would design in dashcam application. The input voltage may have…
Part Number: LM76003-Q1 Hello together,
I have two questions about data, which i cannot find in the data sheet:
1. Can you provide me the transfer-function of the internal OTA used as error amplifier?
2. What is the peak-peak voltage of the oscillator…
Part Number: LM76003-Q1 Hello together,
I have two questions about data, which i cannot find in the data sheet:
1. Can you provide me the transfer-function of the internal OTA used as error amplifier?
2. What is the peak-peak voltage of the oscillator voltage…