Part Number: OPA1656
How do I design Low Noise & Low Distortion Headphone & Small Signal Audio Amplifiers?
Headphone Amplifiers
On-Chip Thin Film Resistors Enable High-Performance Audio Circuitry – SBOA312
Stabilizing Difference Amplifiers…
Hello,
If the ORP sensor output voltage will not go beyond +/-3V then the LM833 will likely work just fine. If it will go beyong +/-3V I do not recommend using the LM833 due to the input common mode range of the device. The input common mode range is…
Other Parts Discussed in Thread: RC4580 , LM833 "Balanced" Mic Pre-Amplifier (PGA2500/INA166?)
Q:
1. Can "bipolar" input and "balanced" be thought of as the same thing?
2. What follow up will I need to narrow down which pre amp…
Other Parts Discussed in Thread: LM833
I refer to AN-346 "High-Performance Audio Applications of the LM833". The overall design procedure is quite clear for me. I only don't catch what magic number 8.058 means (page 5). I'm trying to adapt this design…
Hello Tim,
Thank you for the help. Its a Technics cd player, and the BA4560 is a SOIC package like the LM833. From what you said the the specs the BA4560 would be the most compatible. I am currently downloading Tina. The LM833 just after the MASH DAC…
The LM833 has all the packages that the LM833-N has.
Isn't the LM833D a better match for LM833M/NOPB and LM833MX than OPA1652AID?
LM833MMX/NOPB crosses to LM833DGK
Other Parts Discussed in Thread: LM833 Hey Guys, I am Looking for I2c Controlled addressable stereo volume control IC.
Communication protocol: I2C
Addressable : I need to use four of them
Volume Conteol: Mute also
Earlier I was using a digital pot with…
Other Parts Discussed in Thread: OPA350 , PCM4202 , OPA1632 , LM833 When i use the OPA350 in non inverting configuration with Rg = 2k7 and Rf = 1M
when i feed 5mV to the positive Input via Frequency Generator i Need to set an
DC Offset of 2,5mV to get a full…
Mouser was kind enough to send me the EOL list they had received from TI. I'm not sure I can attach a pdf here so I've linked to it:
www.proaudiodesignforum.com/.../ti_20150901004_09292015_eol.pdf
This is the e-mail address in the cover letter…
I have a customer who is using ADI: SSM2167 (low volt. microphone preamplifier with variable compression and noise gating)
I found the LM833 but it seems to be only part of the solution.
Please recommend a full-cross for this part. Doesn't matter if multiple…