Part Number: LM9061-Q1 Hi
We are using LM9061QDRQ1 in our design. Below is the schematics. We are currently testing our board. And in one board we are observing the gate driver output is rising high but then goes low. What could be the issue. i'm sharing…
Part Number: LM9061-Q1 Hi ti team,
we are using LM9061QDRQ1 gate driver in our automotive application.
it working well and good in initial stage and now we are observing that the delay pin is giving 7v and we checked other gate driver which is same…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM9061 Hi
We are using LM9061QDRQ1 in our design to drive the MOSFET IAUT300N10S5N014ATMA1 for our retarder ECU. Our 24V system max voltage can go till 32V. On checking datasheet the max supply…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM9061 Hi
We are planning to use LM9061QDRQ1 to drive our Mosfet IAUT300N10S5N014ATMA1. We are using this for our Electro-magnetic retarder ECU board. PLease let us know if this gate driver is…
Part Number: LM9061-Q1 Tool/software: Hi,
My question is regarding the use of LM9061-Q1 as a High-side Gate Driver for DC-DC Switching Converters. Can this be used for switching the MOSFET at 100-200kHz?
In this image the output turn-on and turn…
Part Number: LM9061-Q1 Dear sir,
I am planing to using the LM9061-Q1 ic for reverse polarity protection. This ic suitable for the reverse polarity protection or any other ic are there?
Our requirements:
Voltage: 400V DC
Current:7.5A
Power: …
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM5067 Hi, support team
My customer has the questions as follow:
I am looking at your LM9061-Q1 product and I want to use to for its features. However, the datasheet of this product showcases…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM5069 , TPS24720 Hello Sir,
1.) I am using LM9061-Q1 high side gate driver in one of my applications. I have done a calculation for worst case scenario and I am switching a mosfet with this…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM9061 , LM5069 , LM5066 , LM5050-1-Q1 , LM5060-Q1
Dear Sir,
I am using LM9061 for hotswap of two supplies from mains and Battery,to swap the Voltage of 24 Volt. I am using two LM9061 to drive…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: TPS25982 Dear Sir,
Currently, I am using LM9061M_NOPB
Do you have a similar IC which works for Supply voltage: 6V to 9V DC.
Regards Murthy