Other Parts Discussed in Thread: LM96000 I have a customer who is asking for a hardware monitor that has a separate fan failure pin that notifies the user of a fan failure. If I understand this correctly, the LM96000 doesn't have a separate fan failure…
With your guys help we got the I2C working. We are now having issues with the external diode temperature reading. We have copied the reference design but when we try are read either temp diode we get -127C. I have confirmed the diodes are in the correct…
Hi,
I would like to ask you a question about the response time from register setting to PWM out.
Could you tell me the actual time, from PWM register setting to PWM signal is output (PWM output signal is changed.)?
I expect that the actual time…
Other Parts Discussed in Thread: LM96000 Hi,
I have short experience on LM96000 device, so could you please help me to read Tach 16bit register value as below?
I designed LM96000 to monitor temp and control fan speed.
But how can I understand the…
Other Parts Discussed in Thread: LM96000 Hi Sirs:
I have two questions about LM96000.
1. Could you provide the maximum input voltage value on tachometer pin?
2. If the Tachometer pin detect PWM high frequency over 22KHz. What solutions we can add…
1. In case I don't need to use VID, is it OK to float the pins?
2. In case I don't need to use REMOTE2, should the +,- pins be shorted?
3. Is the SMBus compatible with I2C? or are there some limitations?
Part Number: AMC6821 Other Parts Discussed in Thread: LM96000 Tool/software: Hi
Could you help suggest a product that can replace Emc2303, Need to drive 3 fans
Thank you
EMC2301/2/3/5 Data Sheet
Part Number: LM96063 Tool/software: Hi TI team, as you might already know Tacho signal is corrupted when PWM is used to cut the GND connection to FAN. Example circuitry: LM85/LM96000 Evaluation Board User’s Guide
LM96063 datasheet claims that it can…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96000 Tool/software: Hi,
My customer is looking to replace Microchip’s PWM fan controller EMC2305
Requirements: they need at least 2 PWM controllers and 4 TACH inputs
The cross tool recommended…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96000 Tool/software: Hello Team,
We are using the DC blower BFB1112H in one of our applications.
The fan is used in one of the items we have procured from nvent .
MPN - 24572-411
The RPM…