Part Number: LM63 Other Parts Discussed in Thread: LM96000 Hello E2E Experts,
Good day.
Using this E2E post for reference: (+) LM63: Technical inquiry - Sensors forum - Sensors - TI E2E support forums ,
Is it possible to run two instances of the…
Part Number: LM63LM64LM96X63EVM Other Parts Discussed in Thread: LM63 , , LM96194 , LM94 , LM96000 , LM93 Do you have a new version of the LM63 evaluation board that is now compatible with windows 10?
Thank,
Aslam
Part Number: LM94 Other Parts Discussed in Thread: LM96000 Hi Sir,
I would like to survey fan controller with I2C watchdog timer, please check the requirement in below.
Customer can accept multiple solutions if single one can not achieve.
1. 12…
Part Number: LM96063 Other Parts Discussed in Thread: AMC80 , LM96080 , LM96194 , LM94 , LM96000 , LM93 Hi,
We currently have a project for the Intel Q670 platform. We have a total of 4 fans (2x SMART FAN and 2x non-Smart 12V FAN). However, due to the…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96194 , LM96000 , LM93 Hi Sir,
We would like to find FAN speed controller solutions(I2C interface, up to 6-CH is better).
May I have your recommendation on this?
Thank you.
Hi Michel,
Please look at the LM96000, LM93/LM94 or LM96194 datasheets and see if these one of these will work for you. These devices have two remote temperature sensors and should not need calibration with the recommended junctions mentioned in the…
Hi Gregory,
Below is my feedback.
Gregory Duperon said: I have a customer in need of a fan controller similar to the AMC6821 , but preferably a dual version.
If the customer needs at least two TACH and two PWM they can look at the LM96000, LM93…
Hi Nimesh,
I was able to replicate the variation of the PWM duty cycle. This variation is a result of using High resolution mode (register 0x45 bit:4 =1). For more consistent PWM use standard set register 0x45 bit:4 =0.
Also below is my feedback…