Part Number: LM96163 Hello TI team,
I am using the LM96163CISDX/NOPB fan controller in my design and would like to clarify the recommended resistor network for the tachometer (TACHO) input.
The datasheet specifies a 1K - 13K - 10K resistor network…
Part Number: LM96163 Other Parts Discussed in Thread: AMC6821 , Tool/software: Hi expert,
May I have your help to explain more detail what's the meaning of bit0 & bit1 of reg4A?
Customer find when reg03=0x4, and Smart Tach mode is enable, they would…
Part Number: LM96163 Other Parts Discussed in Thread: AMC6821 Tool/software: Hi expert,
Customer used LM96163 with SoC which could only provide 3.573Khz SMBus clocking but our DS spec required 10-100Khz.
Although so far during evaluation stage, customer…
Part Number: LM96163 Tool/software: Hi expert,
Customer used LM96163 but sometimes they would see Alarm Status became 0x7F in about every 100,000 reads however, the measurement of local temp is good not over defined spec, and also we think I2C communication…
Part Number: LM96163 Hi expert,
There is a tHD:DAT spec in DS and defined Data Output hold time. Is there a spec requirement for Data Input hold time after SMBCLK low?
Thanks,
Allan
Part Number: LM96163 Hi expert,
May I know how to set the I2C address for multiple device application? Customer would like to use three sockets per board.
When look at the DS description, it seems all the address bits are programmed internally, and…
Part Number: LM96163 Other Parts Discussed in Thread: LM63 , LM96063 Hi expert,
May I check with you why REG 0x4F the POR value is 0x04 but why default value saying is 10C instead of 4C?
Thanks,
Allan
Part Number: LM96163 Other Parts Discussed in Thread: LM96063 , Hi,
Good Day.
Customer had systems in production which use:
- LM96063
- External MMBT3904 diode (from Diodes Inc.)
He needs to know if there's a way to create equivalent functionality…
Part Number: LM96163 Hi expert,
Customer used LM96163 and has some questions regarding data hold time spec. DS define tHD:DAT = 300ns ~ 1075ns but what customer measured is 2139ns which is over the maximum spec.
What we understand from PMBus2…
Part Number: LM96163 Dear Expert,
We are facing an issue that the register sets are (0x4A) =0x20 and (0x4D)=0x17, but It's still can't adjust the PWM duty by modifying 0x4c (0~46).
The PWM pin level is always high. I can't control PWM duty in manual…