Other Parts Discussed in Thread: LM96194 Hi,
The LM96194 device has a nominal supply voltage of 3.3V. Can this device be used for monitoring 12V supply if the 12V supply is present on the board before the 3.3V supply is generated?
Regards,
Prachi
Part Number: AMC6821 Other Parts Discussed in Thread: LM96194 , LM96000 , LM93 Hi Sir,
We would like to find FAN speed controller solutions(I2C interface, up to 6-CH is better).
May I have your recommendation on this?
Thank you.
Hi Michel,
Please look at the LM96000, LM93/LM94 or LM96194 datasheets and see if these one of these will work for you. These devices have two remote temperature sensors and should not need calibration with the recommended junctions mentioned in the…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96194 , LM94 , LM96000 , LM93 Dear Team,
Can you help on suggesting the suitable device for my customer?
Input : FAN’s present x4 or x8
Input : FAN’s TACH x4 or x8
Input : Thermal interrupt…