Part Number: LM97600RB Hi Team,
My customer uses LM97600 to design last year. But I got this part will EOL.
So, Does TI have a suitable replacement solution to LM97600? my customer application is PC-Base DSO.
they interesting in 5G sample rate and cos…
Part Number: LM97600RB Hello,now we are searching for the A/D converter using for the data measurement. Our requirement is that the sampling rate need to be faster than 1G/s, and the number of input channels need to be at least two. Fortunately, we found…
Part Number: LM97600RB Hello,
I cannot get the ByteAlign and ChanAlign values to become all 1's. I have reconfigured the PLLs, re-read the registers and performed Sync Req's but byte 4 or byte 8 always show up as 0. I have gotten all 1's once but never…
Other Parts Discussed in Thread: WAVEVISION5 Hi,
The EEPROM on my LM97600RB board got overwritten with some bad firmware, which resulted in the VID/PID changing from 0x0400/0x2010 to 0x04B4/0x1003. Although I can load the National Semi or Cypress drivers…
Other Parts Discussed in Thread: WAVEVISION5 Hi,
I use Wavevision5.0.6.465 HS11 with LM97600rb.
I try to reload FPGA bit file with Tools->Hardware access Panel -> Default image for selected hardware -> spio5.5_xc5vsx95t_lm97600.bit
Since this…
Other Parts Discussed in Thread: WAVEVISION5 Hi,
I use Wavevision5.0.6.465 HS11 with LM97600rb.
I try to reload FPGA bit file with Tools->Hardware access Panel -> Default image for selected hardware -> spio5.5_xc5vsx95t_lm97600.bit
Since this…
Hi,
There are four ISE project files (.xise) in the design package provided for LM97600RB. Are they for different purposes or they are different versions of the same project?
Best regards,
Supratim
Hi, I'm trying to make a few modifications to the LM97600RB source code but I just wanted to know a couple of details regarding the storage of data samples in the SRAM when the board is powered up. When does the board start storing the ADC samples in the…
Hi,
I'm using the LM97600RB and I wish to automate the signal capture process based on a trigger so that the board keeps capturing data without having to initiate the capture from WaveVision. However, some of the functions such as the Sync Req have to…