Part Number: LMC6001 Other Parts Discussed in Thread: OPA928 Piggybacking off this question asked and already answered , if the typical input capacitance of the LMC6001 is 2.5pf-3pf (depending on DIP or SO), what is the differential and common mode input…
Hi Zach:
My voltage generator is just several 9VDC transistor batteries connected in series. Like you suggested, I will limit my working voltage to < 50VDC. That is, I will charge my home-made capacitors to < 50VDC. Then, I will use a voltage divider…
Part Number: LMC6001 Other Parts Discussed in Thread: SN74LVC541A , SN74AHC244
Hi, Support Team
LMC6001 and LMC6008 between different channel , but same function?
if yes. as we know LMC6008 is very old parts, Could suggest similar function with LMC6008…
Part Number: LMC6001 Customer Capintec is seeing some date code LMC6001's that have been showing Input Bias Current Drifts. Has this been reported as a known issue? Any feedback would be appreciated.
Part Number: LMC6001 Hi,
Sorry for the basic question. Since the input stage of the LMC6001 is a JFET, the bias current flows in only one direction, and I think it is only the sink. Is this correct?
Best Regards, Hiroshi
Part Number: LMC6001 Hi,
do we still have the spice model of OPA124?
Feedback customer:
I am aware that this is already EOL, but I have a schematic here with the OPA124 that I would like to simulate to compare its performance against alternatives.
Tha…
Part Number: LMC6001 Hello,
How to wash the circuit board of the transimpedance amplifier on the LMC6001 chip after soldering?
Especially interesting the input circuit at the place of mounted installation and the body of chip. PCB material - FR4. Flux for…
Part Number: LMC6001 Other Parts Discussed in Thread: LMH6321 , BUF634 , OPA564 , ALM2402F-Q1 I would like to use TI's LMC6001 is integrate a signal between 3 to 10 VDC, but with 22 micro-A. The problem is to use output from the LMC to drive a st of…
Part Number: LMC6001 Other Parts Discussed in Thread: LM7705 I tried to make a transinpedance amplifier for measuring pA-level current from a photodiode. I confirmed that DC-light signal was shown using an oscilloscope. However, 50Hz signal appeared an…
Part Number: LMC6001 The datasheet specifies the offset voltage for the LMC6001A as follows: Vs= 0V/+5V, Vcm=1.5V: max. 0.7mV @ 25°C, Vs= 0V/+5V, Vcm=1.5V: max. 1mV @ the temperature extremes Vs= +/-5V, Vcm=0V: max. 10mV @ 25°C, Vs= +/-5V, Vcm=0V…