Part Number: LMC6001 Hi,
Is the direction of the offset voltage of the LMC6001 positive or negative? or both possibilities?
Our customers use in TIA.
In their test it looks like a negative voltage offset.
Please let them know, as there is no offset histogram…
Part Number: LMC6001 Other Parts Discussed in Thread: LMP7721 , OPA376 Hi,
I want to use LMC6001 to amplify very low current. Please refer to the attachment. Could you please review my schematic? Or could you please tell me how to amplify very low current…
Part Number: LMC6001 I am design a signal amplifier circuit. But I don't know why my LMC6001 is broken. And here is the basic schamatic.
I am afriad if I give a such large amplification. Cause my signal Ip is really small, it is 0.6uA max. (Ip is…
Part Number: LMC6001 Tell me please,
where I can buy a thermal resistor R1 (Fig.23 of Datasheet) 100kΩ +3500ppm/°C?
Micro-ohms do not support this 137 type of resistors.
is maximum 50k. So, I'm very confused (
Thanks
Part Number: LMC6001 Tool/software: WEBENCH® Design Tools We consider using this OA as a pre-amplifier for very low current APD. However, there are no WEBENCH tools available to estimate the bandwidth of the amplifier. Is there any other low current OA…
Part Number: LMC6001 Other Parts Discussed in Thread: BUF634 , IVC102 , We are using a LMC6001a op amp in an electrometer application for ion detection. Our lowest range is 1e-14 amp and go up from there We are using +/-5V power supplies which are bypassed…
Part Number: LMC6001 Hello,
Regarding to the LMC6001,my customer is asking some question.
They are using this device as I-V amp.
To evaluation their board, they check output with input capacitor (several pF:connecting to between input and GND.) as zero…
Part Number: LMC6001 When using the LMC6001 for high precision applications, is there a preferred PCB material that minimizes amplifier input leakage current? The design will utilize a 6-layer board with two internal ground planes and paying a higher…
Other Parts Discussed in Thread: LMP7721 , LMC6001 , LMC6081 I am design a amplier current for photodiode(UVC sensor), I need a very low Ib(input bias current). So I want to choose LMC6001, but I also want to find a alternative for example LMP7721(LMP7721…