Part Number: LMC6482 Hello, customer has to use LMC6482AIM instead of LMC6482AIM/NOPB due to delivery issue which has Lead finish/Ball material SNPB. Does he need to care anything in solder flow/production has pure SN needs higher temperature solder flow…
Part Number: LMC6482 Other Parts Discussed in Thread: LMC6034 , , TINA-TI Hi E2E forum,
I am working on AC sense circuit with 320Vp AC and 60Hz signal. I am facing a issue with the LMC6482 Opamp IC and LMC6034 both. The Input starting from 0 to 320V is…
Part Number: LMC6482 Hi
I received a package with a label and I try to understand the origin for each one, to be sure that the parts came from greenhock
can you help me ?
CSO = GF6, CCO : GBR, ASO = QAB and ACO = PHL
best regards
florent Lacroix
Part Number: LMC6482 Dears
We have fund a issue when using the LMC6482 as the current sensing amplifier, with single supply(0 - 5V), and input common voltage is very close to ground. the offset is around 20mV (with 10V/V, the output is around 200mV)…
Part Number: LMC6482 In My Application
LMC6482 as a DIfferential amplifier for analog current sensing application, I have received a failure such that opamp 6482 IC, its series resistor 10K got failed along with shunt resistor also open.
Shunt open…
Part Number: LMC6482 Regarding LMC6482IMM/NOPB, Package Type VSSOP.
Would like to test multiple ICs LMC6482IMM/NOPB Package Type VSSOP, on a specific test board that already has the layout for package type VSSOP.
Is there any adapter board (having the same…
Part Number: LMC6482 Regarding LMC6482IMM/NOPB, the following marking is present on the chip:
8AVK
A10
Now, A10 -> mentioned under 'device marking' in datasheet
I understand that:
8 -> mfg year = 2018
A -> mfg month = October
What does…