Part Number: LMC7660 Other Parts Discussed in Thread: TMUX7234 , TL431 Tool/software: Dear TI support team,
Please help me review the schematic of the LMC7660.
Thanks!
Part Number: LMC7660 Tool/software: Hi TI Support Team,
I would like to generate -10V and -5V using the LMC7660 .
If V+ = 5V , will the right-side LMC7660 's pin 5 be at -10V , and the left-side LMC7660 's pin 5 be at -5V ?
If not, could you please…
Part Number: LMC7660 Other Parts Discussed in Thread: LM2775 Hi Team,
Could you provide the ThetaJB thermal resistance value for this part?
Thanks and regards,
Marvin
Part Number: LMC7660 Other Parts Discussed in Thread: TL071H , TL071 , LM358B , LM321LV Originally, I wanted to amplify the voltage of about 0.1V~1.0V using TL071HIDR. So when I looked at the data sheet (6.3) of the TL071H, it said that the minimum value…
Part Number: LMC7660 Hello,
I would like you to confirm about below.
* Could you please give me ESD data of CDM(Charged Device Model) ?
There is decription about HBM, but there is no description about CDM.
BR,
Part Number: LMC7660 Hello E2E Experts,
Good day.
We are losing several hundred dollars a month of final product due to failures in part LMC7660. We are using the part well within the voltage spec of the part (3.5 VDC" and in a "N+1" configuration…
Part Number: LMC7660 Hello,
My customer is using the LMC7660 and wants to know if ceramic capacitors are allowed? The datasheet only mentions electrolytic caps.
If only electrolytic capacitors are allowed, then what are the requirements for them …
Part Number: LMC7660 Hi Sir
i want use LMC7660 to create -5V voltage. but i an not as below circuit is correct or not.
may you pls help me double check?
Bogey
Part Number: LMC7660 Other Parts Discussed in Thread: TL7660 , LM2776 Hi, Can you please tell me the difference between LMC7660 and TL7660? If there is no major difference which one of those parts seems to have a longer availability or is more common…
Other Parts Discussed in Thread: LMC7660 Hi team,
One of our customer is using LMC7660 and getting -1.5V for 4.5V input but the ckts works if replaced with TC77660. Schematic is ok and attached is same for reference. Can you plaese help with your comments…