Part Number: LMD18200 Hello
I am working with LMD18200, my output current is below 1A, 0.3A to 0.6A.
I am measured a fix voltage on cueernt sense output pin, any idea how to work with it current below of 1A., I need a current control of 300mA. …
Part Number: LMD18200 Hello team,
I have 2 questions about the test circuit in the datasheet.
What is the role of 12Ω resistors connected between pin6 and pin10, & pin7 and pin2? Are they just for test cirucuit, and can I omit them in the real…
Part Number: LMD18200 Hi,
The datasheet for LMD18200T/NOPB includes two different variants of the circuit, both called "NDJ" package. One that is vertical (NDJ0011B/TA11B) and one horizontal (NDJ0011E/TA11E).
On page 2, it references NDJ0011B. However…
Part Number: LMD18200 The chip storage temperature described in the LMD18200 chip datasheet is -40°C. Now there is a project storage environment temperature that needs to reach -55 ° C, so I would like to ask, what is the maximum storage temperature of…
Part Number: LMD18200 Other Parts Discussed in Thread: LMD18201 LMD18200/NOPB in short supply.
LMD18201/NOPB is available.
My design does not use the current sense pin. Can I use LMD18201 in place of LMD18200?
Thanks,
Part Number: LMD18200 Hello
Regarding the digital signal: PWM,DIR and BRAKE, the logic voltage can be 3.3V,right?
In data sheet the digital IO is 5V level voltage, There is any reson for that?
Part Number: LMD18200 Hello
I am using FPGA to control on the LMD18200, the Vih(min) of the DRV is 2V, The part will work ok with Vih=2.5V from FPGA to DRV?
The distanse between the FPGA and the DRV is ~5000MIL.
Roi
Part Number: LMD18200 Hello
I operate the LMD18200 with VS=30V, Iout=0.3A
The output capacitor should be 0.3X100uF=30uF? It is ok to assembly 4X22uF(50V) ceramic capacitor?
Roi
Part Number: LMD18200 What is the difference between the T/LF14 and T/NOPB and S?
There are slight differences in some dimensions e.g. T&R in the datasheet resp. I don`t find the S version online at all?
T/LF14 seem to have legs that are bent differently…
Part Number: LMD18200 Hello!
Can you help confirm that the only difference between LMD18200T/LF14 vs LMD18200T/NOPB is the tube package size that they come in and the actual parts are the same? It is strange to me that when I search one part in TI.com…