Part Number: LMD18200 Hi team,
Here's an issue from the customer may need your help:=
The chip storage temperature in spec is –40°C. Here's a case needs to be stored at a temperature of -55°C, so the customer would like to know the limit storage…
Part Number: LMD18200 I need more information about how was performed the Total Dose Radiation Test of this part (D9352LMD18200.pdf), it was performed by former National Semiconductor. I am qualifying this part for space applications, and I need more…
Part Number: LMD18200 Hi support team!
I am looking for a product that can replace the anti-lock phase function of the LMD18200.
Would you give me some advice?
Requirement for motor driver is in below,
VM is 36V more over.
Peak current is 4A…
Part Number: LMD18200 Hi Team, What's the difference between LMD18200T/LF14 and LMD18200T/NOPB? What's the meaning of LF14? From our initial checks, only the package quantity seems to be the difference. Is this the case or are there any other difference…
Part Number: LMD18200 Other Parts Discussed in Thread: DRV8873 I AM WORKING ON PROJECT HIGH CURRENT USING ARDUINO NANO AND LMD18200
WHEN THE MOTOR IS FIRST TIME ON IT GAIN A HIGH CURRENT ALMOST 10A
LMD18200 DATA SHEET SAYS IT CAN BEAR 3A CURRENT MY…
Part Number: LMD18200 Hello,
I use a LMD18200 motor driver to drive a motor. The motor is rated 3A. My aplication is basically a positionning application. The motor is coupled to a gearbox and there is an encoder at the output of the gearbox. The controlled…
Part Number: LMD18200 Hi Team,
In the Supply Bypassing section at page 10 of the datasheet of LMD18200, the recommended TVS diode is P6KE62A having a minimum and maximum breakdown voltage of 58.9V and 65.1V respectively while the maximum supply voltage…
Yeow,
We don't have test data to show LMD18200 thermal performance with a heatsink. You may need to buy a demo board with heatsink from the market and get the test data from your side.
For example: https://usa.banggood.com/3A-75W-DC-PWM-Speed-Adjustable…
Part Number: LMD18200
Hi team,
The customer is using LMD18200. The schematic is in the attachment. VSS is 48V. The max continuous current is 400mA.
TA is less than 80 degree C. The motor is a linear motor.
The issue is as below:
The boards can…
Part Number: LMD18200 Hello,
We are currently running some tests on a LMD18200-2D/883 part and we are seeing some anomalies results but the part still functions. The observations that we are seeing is that when the part is powered with 28V there was…