Part Number: LMD18200
Hi team,
The customer is using LMD18200. The schematic is in the attachment. VSS is 48V. The max continuous current is 400mA.
TA is less than 80 degree C. The motor is a linear motor.
The issue is as below:
The boards can be worked…
Part Number: LMD18200 Good day,
I would like to inquire on the following specifications of LMD18200:
1. Saturation Voltage (upper and lower side)
2. over current protection circuit (description)
3. rush current protection circuit (description)
4. minimum…
Part Number: LMD18200 We are developing a control board with LMD18200 motor driver for a welding equipment application [wire feeder]. The equipment as two functional operative work. In the first one the motor current in costant around 0.6 A max, while…
Hi Tim
Do you have any thermal solution about LMD18200?
This chip in my customer's circuit has thermal problem, they want to know is there any solution with this problem?
Thanks
Star
Other Parts Discussed in Thread: LMD18200 , DRV8701 Hi all. I need another IC instead of LMD18200. My customer would like to know H-bridge motion control over 6A(continuous). The LMD18200 is a 3A H-Bridge designed for motion control applications. I think LMD18200…
Dear sir,
My name is Ketan
I had made one DC motor driver project using lmd 18200 t ic with arduino mc. My program is so simple and working fine. My motor is brushed 24 v DC .
Program is motor fwd and reverse control by two buttons no nc type. Pwm is…
Other Parts Discussed in Thread: LMD18200 Hello,
I am trying to supply Ultrasonic Transducer with AC (30W) through a DC power equipment. To convert the DC to AC I will try to use the LMD18200 :
The input will be an oscillating signal send to the DIRECTION…
Other Parts Discussed in Thread: LMD18200 , DRV8829EVM , DRV8829 Hi,
I m using LMD18200 for stepper motor chopper mode drive. I m using PWM control with fixed off time control.
My input voltage to chip is set at 12V, my motor R-4ohm, L-8mH. Motor coil current…
Other Parts Discussed in Thread: LMD18200 , DRV8870 , DRV8842 Hello,
I was inquiring to find out if more information is available about the UVLO feature of the LMD18200? I have reviewed the datasheet and the application report. I wanted to know what parameters…
Hello,
can you please advise regarding a customer complaint about purchased motor drivers LMD18200T/LF14 ?
The customer purchased these already previously and their leadform was according to the datasheet.
but the last dleivery we shipped them shows a…