Part Number: LMG1020 Other Parts Discussed in Thread: THS4303 , THS4302 , OPA858 , OPA855 Hello,
I'm looking for a TI amplifier that could boost a 1ns, 200mV pulse up to the required turn-on voltage at the IN+ pin of the LMG1020, assuming that the IN- pin…
Part Number: LMG1020 Other Parts Discussed in Thread: LMG1210 , LMG1205 , LM5113 , LM5114 Hello, TI experts,
I tried to simulate a power converter circuit with real TI LMG1210 gate driver pspice model in cadence virtuoso environment.
Saw this error when I…
Part Number: LMG1020 Hi team,
The LMG1020 chip specification book mentions that the chip IN and OUT pins can withstand -0.3V, what is this -0.3V in the form of voltage, constant voltage or pulsed voltage?
thanks
Part Number: LMG1020 For Propagation delay in Switching Characteristics, TEST CONDITION is IN-=0V, IN+ to OUTH,OUTL, Is tpd equivalent for IN+=Vdd, IN- to OUTH,OUTL? Or is there a difference?
Part Number: LMG1020 Hello,
I ran a simulation with LTspice using a PSpice model of LMG1020 provided by TI.
The schematic is as follows.
As a result of the simulation, the output voltage Vout is about 1.97 V as follows.
But, the output voltage should…
Part Number: LMG1020 Hi team,
I want to find a VCSel driver which has below specs.
LVDS differential input, single channel.
LVDS input frequency is larger than 10Mhz.
Pulse current is larger than 5A and the pulse time is shorter than 2ns.
MOSFET integrated…
Part Number: LMG1020 Hello,
I'm carefully reading the decoupling recommendations of the LMG1020.
In the datasheet :
Figure 16 presents a layout of LMG1020 with a 0.1 µF feed-through capacitor (C1) and a larger 1uF capacitor (C3) for decoupling. In…
Part Number: LMG1020 spike_pulser.pdf
Hello,
I'm running tests for generating negative short pulses.
Expected pulse output is 5ns width pulse from 0 to -200V.
However, as a result of the test, only the output of about -10V coms out. And the pulse…
Part Number: LMG1020 Hi Team,
Good day! I need your expertise with reviewing the schematic of our customer.
They are trying to use the LMG1020 to drive DMN1250UFEL MOSFET. The OUTH and OUTL are shorted together through a resistor going to the gate of the…
Part Number: LMG1020 Hi,
Good Day. I have a customer who is working with LMG1020. Please see below the query of our customer for your reference. Thank you very much.
I want to ask a question about LMG1020.
Based on data sheet, it can burst gate of n-channel…