Hi Walter Zollinger
I am encountering a similar issue with an application using the TI LMG1210EVM-012 board.I believe my question could benefit others in this discussion thread as well.
**Project Objective:** - Use two LMG1210EVM-012 boards in a full-bridge…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 We are having difficulty testing the LMG1210EVM-012, we are using a 10 Volt power supply for the input bias supply, 20 volt for the input DC supply while PWM signal within a range of…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 Hi Support Team
We are using LMG1210EVM-012 evaluation board.
Following are the input provide.
1. Providing +5V to LM1210 pin 4 via TP1 ( +5V DC ) and TP4 ( GND )
2. Providing +42V DC…
I have replaced the device twice, and I am still seeing 11.74 on VDD. What are the implications of leaving both DHL and DLH floating? I have no use for the internal LDO otherwise.
Per part U1.5, the Bootstrap diode is capacitively coupled to HS via a…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 Tool/software: WEBENCH® Design Tools Dear Lixing Fu
Can you send me a link to LMG1210EVM-012 Gerber files and BOM in Excel format?
I need to make a layout of multiple channels with EPC2034…
Hello Tony,
I contacted the engineer who designed the TIDA-01634 and researched to find the design files. I was not able to find the files for this particular reference design.
The engineer who designed this reference design referred us to the LMG1210EVM…
Part Number: LMG1210 Tool/software: Hi,
I'm using LMG1210 as half bridge driver in one of my applications in which I want switching frequency is between 1-1.5MHz. For cost saving I'm using AOD2544 MOSFET instead of using GaN FET. In half bridge configuration…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 If I give -200V at input i.e. V(HS) will be -200 and PGND will be connected to GND.
In this case I will need to remove the bootstrap diode and give V(BST) from an external isolated s…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 , LMG1020 I need to generate pulses with 10ns pulse width at 200V .
Can I modify the EVM circuit by changing the GAN FETs and Bootstrap diode to 200V specs?
Will there be any issues that…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 , UCD3138 The LG1210 Power stage has a capability of operating up to 50MHz.
But you give no indication of a PWM control that will take advantage of this high frequency.
Can you recommend…