Part Number: LMG3410-HB-EVM Hi,
Customer use our EVM for testing, and they use voltage source to provide HVBUS voltage, but they see when without load, the HVBUS=400V, current through HVBUS is 35mA, it looks big.
Do we have power consumption data for…
Part Number: LMG3410-HB-EVM Other Parts Discussed in Thread: LMG3410R150 Hello we are testing our LMG3410-HB-EVM motherboard with LMG3410R150 daughter card. We biased the card then the FAULT LED and AUX_ENABLE LED is ON.
After that we connected the load…
Part Number: LMG3410-HB-EVM Hi,
I am looking into a interesting fact of LMG3410-HB-EVM: The !FAULT output is routed to adjust the slew rate of low-side FET. What's the consideration under this design?
Peiheng.
Part Number: LMG3410-HB-EVM I am using this daughter card for a Dual Active Bridge DC-DC converter of the 250kHz switching frequency. I can not increase the DC bus voltage above 140 V even at 50 W power level. The fault signal is being generated and the…
Dear Sam,
Please see below for the specific evaluation module (EVM) that you can purchase.
http://www.ti.com/tool/LMG3410-HB-EVM
http://www.ti.com/tool/lmg34xx-bb-evm
We do have a lot more reference designs online with design info and test result available…
Part Number: LMG3410-HB-EVM Hi,
My customer can' t open cad files of LMG3410-HB-EVM.
Which tool did you use when you design this EVM?
Best Regards,
Ted
Part Number: LMG3410-HB-EVM Hi,
I bought the LMG3410-HB-EVM Half-Bridge and LMG34XXBB-EVM Breakout Board EVM. I'm trying to use parts of these to build a pcb of my own. The altium files online seem to be read only, and I don't have access to the pcb libraries…
Part Number: LMG3410-HB-EVM Customer is evaluating LMG3410-HB-EVM (and LMG3410-BB-EVM), but L2(inductor) was increased over 120℃ by thermograph.
User's guide is described that heatsink and airflow are recommended, but I think these idea is not critical…