Part Number: UCC25630-1EVM-291 Other Parts Discussed in Thread: LMG3410-HB-EVM Serkan-san,
I tried your proposal.
I just only changed Si MOSFET to LMG3410-HB-EVM according to your proposal.
But did not work.
RVCC does not up to 12V.
Do you have any idea…
Part Number: UCC25630-1EVM-291 Other Parts Discussed in Thread: LMG3410-HB-EVM , Hi all,
I have UCC25630-1EVM-291 and LMG3410-HB-EVM.
I want to change the LLC Mosfets Q1,Q2 from two SPW20N60CFDs to two LMG3410s.
Use LMG3410-HB-EVM as is OK. Primary 5V is…
Part Number: LMG3410-HB-EVM I would like to use the LMG3410-HB-EVM with a +3.3Vdc supply.
In the reference design, the isolation transformers (T1 and T2) have a 1.3:1 turns ratio (P/N 760390014), such that with a +5Vdc supply the output voltage is ~14…
Part Number: LMG3410-HB-EVM
We have made some improvements to the LMG3410-HB-EVM, resulting in a revision D of the EVM. The official EVM Users Guide is currently being modified, so this document acts as an errata until the formal documentation is complete…
Part Number: IWRL6432 Hi Team,
I got segmentation fault when building project with Linux CCS. Could you advise how to debug this issue?
Building target: "motion_and_presence_detection_demo_xwrL64xx-evm_m4fss0-0_freertos_ti-arm-clang.out"
Invoking: Arm…
Hi Sravan,
You have listed 3 possible solutions
Buck + HB-LLC
Buck + HB
HB only
The decision to use one or the other depends on how important efficiency is compared to complexity. I would recommend LLC since the gains in efficiency and performance can…
Ochi-san,
1. We offer TPS1HC100EVM and TPS1HC30EVM. For any other devices, please contact the team directly. HC devices are not meant to be used with the motherboard evm.
2. We do not offer TPS2HB08-Q1. The lowest RON device is TPS1HB08-Q1.
3. The motherboard…
Hi Bo, Typically the board-evm.dts is used for U-Boot stage & corresponding board-evm-u-boot.dtsi is used for SPL stage. Example: board dts: https://git.ti.com/gitweb?p=ti-u-boot/ti-u-boot.git;a=blob;f=arch/arm/dts/k3-j721e-common-proc-board.dts;h=1b600547c064f852241e4c93b0dfbcebca090e9a;hb…
Part Number: PROCESSOR-SDK-AM335X Hi Expert,
We have one custom board which is based on AM335x-evm processor.
Currently, we have 2013.01.01 U-Boot SPL with Linux version 3.2.0 and it's booting successfully.
But, we planning to migrate 5.10.184 Linux…
Part Number: LMG3422R050 Other Parts Discussed in Thread: LMG3422R030 , LMG3410-HB-EVM Please kindly advice Drain slew rate v.s. Drive Strength resistor curve both LMG3422R050 and LMG3422R030?
Here is example of LMG3410-HB-EVM