Part Number: LMG3410EVM-018 Other Parts Discussed in Thread: LMG3410R050 Hello,
I am planning to use LMG3410R050 EVM for phase shifted full bridge operation. As far as i understand there is no reverse recovery diode in LMG341x family devices and in the…
Part Number: UCC28019A Other Parts Discussed in Thread: LMG34XX-BB-EVM , LMG3410EVM-018 , , ISO7731 , LMG3410EVM-031 hi,
Customer try to use UCC28019A EVM + LMG3410EVM-018 + LMG34XX-BB-EVM to test GAN.
do you have suggestion how to connect these evm?
BR, …
Part Number: LMG34XX-BB-EVM Other Parts Discussed in Thread: LMG3410EVM-018 Hello,
I am using LMG34XX-BB-EVM with LMG3410EVM-018. DC input 300V, 12V isolated dc input and no load at the output(just a multimeter). I am using LaunchXL28379D for PWM input…
Part Number: LMG34XX-BB-EVM Other Parts Discussed in Thread: LMG3410EVM-018 Hi,
I am currently working on LMG34XX-BB-EVM and LMG3410EVM-018 for a DC DC converter application. As i see from the schematic AGND and PGND is connected via R9.
Is it possible to…
Part Number: LMG34XX-BB-EVM Hello,
I am using LMG34XX-BB-EVM with LMG3410EVM-018 . On page 7 of SNOU165A, it says that "The LMG34XX-BB-EVM has the following features and specifications: Requires only a single 0V to 5V PWM input to generate gate drive signal…
Hello Zou,
The thermal pad is what you see on page 27 as a large PAD, and page 35 is the pad with thermal vias, where the 10 pads you see is the thermal paste. You can download the CAD model from our website: https://www.ti.com/product/LMG3410R050#design…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3410EVM-018 , Hi Sir,
May I learn from you that could we get free LMG3410EVM-018 Half-Bridge for customer emulation?
Also, Could you share LMG3410R050 SIMPLIS model to us?
Thank you.
Best regards…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3410EVM-018 , PMP20873 Dear Martin
I have 2 questions
The power device LMG3410R050 has a rating of 12Amp, while the daughter board of the same power device (LMG3410EVM-018) has a rating 8Amp…