Part Number: LMG3410R050 Hi experts,
I'm designing a VSI using GaN switches. My question lies in the PCB layout. As stated in EPC and GaN Systems white papers, the best layout practice is to use a 4 layer board, use top layer for VDC+ and mid-layer1 for…
Part Number: LMG3410R050 Hello community
I have assembled a daughter board with upper and lower LMG3410R050 for my motor drive application.
The design isbased on the schematic and values of the switch datasheet. The issue is, when the VDD is connected…
Part Number: LMG3410R050
What is the minimum VDS in which GaN can operate ?
We will have voltage of around 0.75V to 1.5V on the drain terminal. What is the max Drain to source current I can drive from LMG3410R050 GaN device ?
Regards,
Bhanuprakash…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG1210 Designing a 5kW powersupply using a half-bridge configuration...looking into switch/driver solutions and considering the LMG341X family of parts.
Is there a recommended PN within this family…
Part Number: LMG3410EVM-018 Other Parts Discussed in Thread: LMG3410R050 , Hello,
I want to order LMG3410R050 daughter card (LMG3410EVM-018) from ti store. I want to order 4 but there is a limit of 1 item. what do you suggest?
Thank you
Murat
Part Number: LMG3410R050 Other Parts Discussed in Thread: UCC28740 , UCC28780 If I want to use UCC28740 as Flyback controller, and use the LMG3410R050 to replace the MOSFET, to make the solution smaller. Is it possible and anything that needs to be considered…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3410-HB-EVM , LMG34XX-BB-EVM Hi,
I am trying to make a high voltage buck converter ( 400Vin to 300Vout, 4A) using the following circuits.
- LMG3410-050 daughter card (LMG3410-HB-EVM) - LMG34XX-BB…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG1020 Hi
For the LiDAR system, very high current pulse for the LD driving is necessary.
And the max current is depends on the target distance to detect.
Now I'm developing long distance LiDAR…
Part Number: LMG3410R050 Sir,
I am designing 2.5 KW High Frequency XRAY Machine . My XRAY frequency will be 50 kHz . I need to convert DC voltage into 50kHz AC Square Wave . Then i will feed this ac into a transformer.
Can i use LMG3410R050 ? But My current…
Part Number: LMG3410R050 When Turn off, the rising edge of Vds is , Several microseconds and abnormally slow n Is there somewhere a misconnection of the terminal?