Part Number: LMG3410R050
Key highlights and features:
5kW bidirectional AC/DC grid converter using GaN
Achieves 99% efficiency, with no forced air cooling
Supports bus voltages up to 1400V
Features LMG3410R050: 600V 50mΩ GaN with integrated driver and…
Part Number: LMG3410R050 Hi
Our GaN devices doesn’t have body diode so I think that freewheeling diode is required for CCM PFC design.
Is my understanding correct ?
If yes, would your recommendation for freewheeling diode SiC diode ?
Thank you…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG1210 , LMG5200 , My customer plan use GaNFET do DC48V 600W Class D amplifier , Is this feasible? How to achieved ?
James
Part Number: LMG3410R050 Other Parts Discussed in Thread: UCC28070 If I want to use the LMG3410R050 in CCM Interleaved PFC. Anything that needs to be considered?
Part Number: LMG3410R050 Turn off no tachiagari sokudo ga sū m sec to ijō ni osoi nodesuga, do k o ka no tanshi no settei ga warui nodeshou ka? Soretomo debaisu furyōdeshou ka?
Part Number: LMG3410EVM-018 Other Parts Discussed in Thread: LMG3410R050 Hello,
I am planning to use LMG3410R050 EVM for phase shifted full bridge operation. As far as i understand there is no reverse recovery diode in LMG341x family devices and in the…
Part Number: LMG3410R050 Hello,
is there possibility to parallel LMG3410 to increase maximum current?
We are investigating possibility to use LMG3410R050 in our 3-level 3-phase current inverter but we have two options
- pure GaN transistors so we can…