Part Number: LMG3410R070 Hi There,
Am I able to obtain theTI the FIT or any other reliability data for the LMG3410R0x0? This will allow my customer to do some analysis to determine theirproduct's lifetime.
Regards,
Part Number: LMG3410R070 Other Parts Discussed in Thread: ISO722 While using the GanFET at Half- Bridge configuration, we started getting random Fault signals and FET Shuts down
After further investigation we found out that fault caused by the Half…
Part Number: LMG3410R070 Hi!
The datasheet of the LMG3410R070 suggest using C3D1P7060Q as bootstrap diode for hardswitching applications.
That part is however now obsolete. What new part would you recommend?
I have so far used IDL02G65C5XUMA2…
Part Number: LMG3410R070 Questions relate to information given about the LMG3410R070 requirements relating to the ground planes and source connection regarding termination of bypass capacitors and the boost inductor. From data sheet - SNOSD10F –APRIL…
Part Number: LMG3410R070 Other Parts Discussed in Thread: LMG3422R050 Hi There,
I have a customer designing with LMG3410R070 and have a question on the LMG3410R070 at higher voltages. Essentially we want to know if we can run this 600V rated part…
Part Number: LMG3410R070 Hi team,
Does the current flowing in RDRV affect the drain-source current? Or is it adjusted to be constant? I am wondering if the voltage across the RDRV resistor terminals fluctuates.
Sincerely. Ryu
Part Number: LMG3410R070 Hello experts,
for an onboard charger design, we are having 3.3kW Single PFC (using totempole pfc as front end) and followed by PSFB. Now planning to do incremental design for 3 phase with 11kW power capacity. Since the component…
Part Number: LMG3410R070 Other Parts Discussed in Thread: UCC28950 Hi Team,
Did TI have the reference design of UCC28950+LMG341X ?
My customer has a new project and needs support, thanks.
Condition:
Input: 180~425Vdc
Output: 12V/1500W
Part Number: LMG3410R070 Other Parts Discussed in Thread: TIDA-010062 , Hi,
We are developing totem pole bridgeless PFC which based on TIDA-010062. The GAN just use LMG3410R070 demo board LMG3410-HBEVM for high frequency switch. In our test, we found…