Part Number: LMG2610 Other Parts Discussed in Thread: LMG3411R050 , LMG3411R070 Hi,
We need to design a Buck converter with the following specs:
Vin 400VDC
Vout adj. 250VDC to 350VDC
Iout 1.7A max@350VDC, less at lower voltages
Would you recommend LMG2610…
Part Number: LMG3411R050 Other Parts Discussed in Thread: LMG1210 Hi,
I was going through the article that was written on ti website about using a single pwm to control two GaN fets in a half bridge configuration with dead time here .
I also read that when…
Part Number: LMG3410-HB-EVM Other Parts Discussed in Thread: LMG34XX-BB-EVM , , LMG3411R050 Hello, I have set up my power board to use the above half-bridge demonstration board for a PhD project. When I apply a 5V power supply to the demo board, the LED…
Hello Ninomiya-san
A4/ Switching at 300kHz is possible - the PMP20657 runs at this speed - http://www.ti.com/tool/PMP20657
A5/ The LMG3411R050 device can be used with the UCC28951(0) - The LMG3411R050 includes on-board drivers. The 0/10V output of the…