Part Number: LMG3422R030 Tool/software: When I use LMG3422 for half-bridge switching of inverter, there is a significant overvoltage oscillation in the DS voltage, when GAN FET is turned on. Below is my application schematic and DS waveform. What could…
Part Number: LMG3422R030 Tool/software: Hi Team,
Currently, when customer doing reverse test find that the Vsd is quite smaller than its value in the datasheet, which is shown as below:
Input Current
Ambient Temperature ℃
Voltage V
Current…
Part Number: LMG3422R030 Tool/software: Customer is interested in the TI GaN, however there're two questions here.
1. Are TI GaNs able to be connected in parallel? Is there application note or guidance?
2. Customer worried that their SMT process…
Part Number: LMG3422R030 Hi Team,
I want to confirm if the LMG342x and LMG352x can meet the request of 2-4kW scene? The power parameter in roadmap is >1.5kW, does this power parameter mean load power? Thanks.
...
Best Regards,
Ryker
Part Number: LMG3422R030 Hi
I want to connect two LMG3422R030 in series to increase the voltage rating my questions is : 1- Can I connect them in series or there is any issue doing it?
2- My main objective is to connect them in series and not only get…
Part Number: LMG3526R030 Other Parts Discussed in Thread: LMG3422R030 , LMG3522R030 Hi, Could you please share the separate Eon and Eoff data curve for LMG3526R030, or LMG3522R030? Even for LMG3422R030, its Eoff data is hard to extract from the datasheet…
Part Number: LMG3422R030 I am working on a T-NPC type Vienna rectifier. I would like to use a pair of LMG3422R030 back-to-back with their sources connected like shown in the following diagram, one pair for each of the 3 phases. I plan on driving the gate…
Part Number: LMG3422R030 Hello,
I've used LMG3422R030 GaN device to design Hybrid-ANPC inverter
I read the datasheet about LMG3422R030, but I couldn't understand why the GaN switch turns on with the 0V(Source)?
PWM is "IN", Source is "0V", and…