Part Number: LMG3422R050
Tool/software:
Hello, I have a problem with very strong heating of transistors when supplying PWM with a frequency of 2MHz, although the current consumption approximately corresponds to the graph:
Heating occurs when the…
Part Number: LMG3422R050 Tool/software: Hi
We would like to design a converter, and we need to specify the power topology. Please check the specifications below.
Input: 220VDC to 550VDC
Output 48VDC
3kW total power
Please let me know if you…
Part Number: LMG3422R050 Hello dear TI support team, is it possible to get the Altium Designer project for the LMG3422R050 600-V 50-mΩ half-bridge daughter card? Thank you and best regards, Michael Robrecht
Part Number: LMG3422R050 Tool/software: Hello TI support team, is it possible to get the Altium Designer project file for the LMG3422R050 600-V 50-mΩ half-bridge daughter card? Thank you, Thomas Price
Part Number: LMG3422R050 Other Parts Discussed in Thread: LMG3422R030 I am trying to run a simulation of LMG3422R050. I have downloaded the simulation model from TI's website and opened the model in PSpice for TI. When I try to run the model I get a bunch…
Part Number: LMG3422R050 Tool/software: Hi Experts,
Can you help us evaluate this concern from customer using LMG3422R050 in switched-capacitor circuit ?
See attached the description of my question in details to this email. This is confidential. …
Part Number: LMG3422R050 Other Parts Discussed in Thread: LMG3522R050 , Tool/software:
ジャンクション・パッケージ上面の熱抵抗(赤い斜線で示しています)はデータシートに記載されていませんが、そのデータはありますか?また、ジャンクションとパッケージ上部のジャンクションに最も近いポイントとの間の熱抵抗に関するデータはありますか?もしそうなら、ご指導をお願いいたします。
Part Number: LMG3422R050 I was going through the data sheet of LMG3422R050 and couldnt find the
Reverse Transfer Capacitance and internal gate resistance if there is any.
Could you please help me?
Best Regards,
Arjun Ananthaiah
Part Number: LMG3422R050 Hi ti team,
The customer is looking for a GaN solution: PFC+LCC. Input is 380V-400V, output is 24V with 25A, please help recommend suitable TI models, Thanks!