Part Number: LMG34XX-BB-EVM Hi. We are trying to acheive the rise time and fall time <=2ns at 200V. We want to know if it is possible with this board (we can provide subnanosecond rise time pwm signal)
Part Number: LMG34XX-BB-EVM Other Parts Discussed in Thread: TIDA-00909 , TIDA-00913 , TIDM-02008 , TIDA-00915 , TMDSSOLARUINVKIT , LMG3410R150 , LMG3410R050 , TIDA-01606 I have seen LMG34xx GaN system-level evaluation motherboard, can you explain "this EVM is…
Part Number: LMG34XX-BB-EVM I buy LMG3410 HB EVM and LMG34XX-BB-EVM board, and use them together
I am using 3 phase power supply to supply DC power through 3 phase diode rectifier.
The PWM signal uses a BNC connector and supplies a 12V supply to the LMG34XX…
Part Number: LMG34XX-BB-EVM Other Parts Discussed in Thread: LMG3410-HB-EVM , TIDA-00915 , LMG3410R050 , LMG3410R070 Hi,
We did not manage to know the maximum current rating of LMG3410-50
The design of TIDA-00915 & The EVM LMG3410-HB-EVM allow us to know…
Part Number: TRF371125EVM I followed the instruction for the EVM test in the datasheet.
The current that the board runs is 290mA instead of 385mA in the datasheet.
When I checked using a spectrum analyzer, the mixer itself worked, but the BB amp did not…
Part Number: LMG34XX-BB-EVM Other Parts Discussed in Thread: LMG3410-HB-EVM I buy LMG3410 HB EVM and LMG34XX-BB-EVM board, and use them together
I am using 3 phase power supply to supply DC power through 3 phase diode rectifier.
The PWM signal uses a BNC…
Hi Andreas,
Just want to update my progress. Finally I manage to build Linux OS using custom machine configuration. I realize that am62xx-evm-k3r5.conf is needed by am62xx-evm.conf (not sure where bb file that connect both of them). So I need to create…
Hi David,
Lets take a couple of steps back.
1) are you trying to build sysbench application from the recipe available in meta-openembedded (./meta-openembedded/meta-oe/recipes-benchmark/sysbench/sysbench_0.4.12.bb)?
2) are you trying to build this for…
Part Number: SK-AM64 Hi,
We are using SK-AM64 EVM board. We wanted to add Coovachilli - captive portal package on to the target. We understood that, to add new packages to the target, we should need respective bitbake files.
Is there any other way to add…
Hello,
All of the things I mentioned about our LMG3422 devices also apply for the LMG3410. It can be used as a synchronous rectifier and the EVM you referenced can be configured as a synchronous buck or boost converter using the LMG34XX-BB-EVM .
Regards…