Part Number: LMG5126
The datasheet doesn't mention heat sinks at all. It doesn't really include any information about thermal considerations at all actually. What's the best way of mounting a heat sink on top of the device? Just bolts, or a spring clip…
Part Number: LMG5126 Hello,
I found in datasheet information that LMG5126 XSE5126 ICs have a problem with "thermal shutdown." procedure. Do you know if in silicon XTS5126 this problem is solved? Or do you still see any potential burn problem in case…
Part Number: LMG5126-CALC Other Parts Discussed in Thread: LMG5126 , LMG5126EVM I’m currently working on a new design where we will use the following device: LMG5126 We would like to use the corresponding EVM PCB layout as a reference.
Could you please…
Part Number: LMG5126 Tool/software: Hi all,
I am interested in the LMG5126. I saw the data sheet of the LMG5126. I understand that it is a boost DC with a built-in GaN FET.
What is the target application of this device?
”2 Applications
• High…
Part Number: LMG5126 Hello team,
Since my customer cannot find power-up sequence in datasheet, they want to double check that is there any power-up sequence. Can you also check pre-bias(e.g. Vin=12V/Vout=30V) start-up is problem or not.
Regards, …
Part Number: LMG5126 Tool/software: Hello team,
My customer want to know maximum power with heat sink. I understand it's strongly depend on their cooling system, but can you show as their reference?
Condition 1: Vin: 12V, Vout: 40V, Fsw=480kHz Condition…
Part Number: LMG5126 Other Parts Discussed in Thread: LM5155 Tool/software: Hello,
My customer is looking for DC/DC boost ICs that can support the following conditions.
CASE1 - Input : Battery 3.7V / 10A, Output : 28V / 7A
CASE2 - Input : Battery…
Part Number: LMG5126 Tool/software: Recently we started a booster design and must now decide whether or not it can be based on the LMG5126.
Does anybody know when this part will be available?
Part Number: LMG5126
Tool/software:
Need the package footprint drawing VBT0022A VQFN-FCRLF 22 - the LMG5126 datasheet provides a hardly readable pixel image only.
Can't find the LMG5126 for sampling and buy
Part Number: LMG5126 Other Parts Discussed in Thread: LM5171 Tool/software: I have a design with the specifications below:
Input voltage min: 9V Input voltage nominial: 20V Input voltage max: 28V Input current max: 16.5A @ 20V Input current >= 5A @…