Part Number: LMG5200 The part is marketed as a "10 A" Half-bridge power module. Yet, the abs. max. rating mention 10 A as the unconditional switch node current, which would turn it rather into a "5-6 A" half-bridge module when accounting for realistic…
Part Number: LMG5200 Hello,
We are incorporating the LMG5200 as a sine wave source that doubles as a power supply and a FM command communication source. We had issues with the LMG5200 blowing up in our first layout, we suspect this was because we missed…
Part Number: LMG5200 Hi Folks,
It's been a while and I've gotten no response from my previous post. I've had another failure that I suspect is related to the VCC input toggling, so hoping to have my previous question answered. This time around…
Part Number: LMG5200 Hello,
TI's datasheets are usually very well drafted and highly consistent. However, this one left me wondering. O n several occasions, the datasheet mentions VSS/VDD related information:
Table 1 mentions "V CC - V SS " …
Part Number: LMG5200 I am using a 7V VIN and it seems like to switching frequency is affecting the VIN. Even at a slow frequency of 200Hz, the VIN is affected by the switching. I see periodic dips on the 7V whenever HI goes high and LI goes low.
Part Number: LMG5200 Hi,
The customer plans to use the LMG5200 for stepper motor drive. I don't think GaN FETs have body diodes, should I take measures externally? If I need a diode, which is better, SBD or FRD?
Best Regards,
Nishie
Part Number: LMG5200 Other Parts Discussed in Thread: BOOSTXL-3PHGANINV hi,
a customer is evaluating LMG5200 via BOOSTXL-3PhGaNInv EVM. they use external SOC to control BOOSTXL-3PhGaNInv EVM. they wants to know what is the maximum operation frequency…
Part Number: LMG5200 Hello,
We are using the LMG5200 half-bridge modules in a multiphase GaN inverter for motor drive applications. When driving a simple three-phase inductive load (1mH load), we are observing undershoots on the switch node outputs exceeding…