Part Number: LMG5200EVM-02 Hello Team,
I have 2 questions:
1) Can the efficiency be at 45% for these conditions: Vin = 48V; Vout = 5V; Iout = 0.5A; Fsw = 2.5MHz ?
Measured input power 5.5W output power: 0.5A x 5V = 2.5W
So power losses of 3W are bigger…
Part Number: LMG5200EVM-02 Other Parts Discussed in Thread: TINA-TI , LMG5200 Tool/software: TINA-TI or Spice Models Hello,
I have this board with me and I want to simulate it in PSpice before testing it in the laboratory. The Spice model I downloaded from…
Other Parts Discussed in Thread: LMG5200EVM-02 부품 번호 : LMG5200EVM-02
I ran two lmg5200-2 evm boards in the same environment and one board does not work. It was operated in the same environment and there were no strange symptoms such as smoke or noise…
Part Number: LMG5200EVM-02 Other Parts Discussed in Thread: LMG5200 , C2000WARE Tool/software: Code Composer Studio Hello, currently I'm using the LMG5200EVM-02. I want to create a PWM Signal and I'm using following code:
volatile unsigned long…
Part Number: LMG5200EVM-02 Hi Team, I am posting this inquiry in behalf of my customer. 1. an this board be used for the following application: A buck converter working at 1MHz switching frequency and input voltage of 3.3V output voltage of 1.8V and load…
Part Number: LMG5200EVM-02 Other Parts Discussed in Thread: LMG5200 Hello,
While testing the board at switching frequencies (1 Mhz and 10 MHz) with variable load resistor of 0 to 36.3 ohms, the high side GaN Mosfet failed. I measured the input impedance…
Part Number: LMG5200EVM-02 Other Parts Discussed in Thread: LMG5200 Dear Master,
I use LMG5200EVM-02 to verify 5Mhz but waveform become very strange and efficiency down to 84%(original all over 92%).
Dut to I need to verify differently inductor,the test…
Part Number: LMG5200EVM-02 Other Parts Discussed in Thread: LMG5200 Hi
i try to operate the LMG5200EVM-02 but there is no output signal.
the output load is resistor of 47 Ohm.
On step 1 : I Connect a Supply to J3 Connector (6V).
On step 2 : I Connect …
Part Number: LMG5200 Hi Team,
A customer would like to know the difference between the LMG5200EVM-01A and the LMG5200EVM-02? As far as I can see, they are the same and I couldn't find any differences.
Regards,
Mihir Gupta
FAE - South Germany
Hi Tosi,
For V3, you will be connecting it as show in the LMG5200EVM schematic shown in the user's guide ( https://www.ti.com/lit/ug/snvu551/snvu551.pdf?ts=1643211241238&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FLMG5200EVM-02 ). V3 will…