Part Number: LMG708B0 Hi sir,
Pls provide LMG708B0 Orcad Symbol / Footprint.
Customer needs the info to pass the AVL and start the design, thanks a lot!
Part Number: LMG708B0 We obtained an LMG708B0-EVM12V board and measured its full load power conversion efficiency. Our measurements fall 1.3% to 2.1% short of the values claimed in the EVM User's Guide: LMG708B0-EVM12V (latest revision, April 2026), page…
Part Number: LMG708B0 Hi,
I've purchased the LMG708B0-EVM12V and it looks to be great for our application. Would it be possible to purchase 10 samples of the LMG708B0 for further testing? If so can you please point me to the correct contact.
Regards…
Part Number: LMG708B0 Hello,
there appears to be a fault in the preliminary datasheet SLVSJL4.
On page 21 equation 11 provides a way for calculating the average output current when using IMON for current monitoring.
The I_CC in the denominator should…
Part Number: LMG708B0-EVM2PH Hello Team,
I encountered a failure while testing the LMG708B0-EVM2PH .
Test Conditions:
Input Voltage: 50 VDC
Input current limit set to 10 A
Output Voltage: 12 VDC, Elec. Load 30 A
Maximum output power was…
Part Number: LMG708B0 I am looking to connect with someone on the LMG708B0 team. Late last year I selected the LMG708B0 as a candidate for a new design. In early January I opened support tkt to purchase samples and an eval board. Although I have followed…
Part Number: LMG708B0-EVM12V We would like to use
LMG708B0
for an FPGA (Ti375) based power supply. Therefore I would be grateful if you send me the altium project files and the datasheet.
With my best wishes and regards.
Part Number: LMG708B0-EVM12V Other Parts Discussed in Thread: LMG708B0 , Hi Team,
We are currently working with the LMG708B0-EVM12V evaluation module and planning to develop a custom design based on the LMG708B0 device.
We request your support in…
Part Number: LMG708B0 Dear,
Good day!
I want to check below information of PLMG708B0VBTR / LMG708B0VBTR . 1. Wafer Size/ Process Node(ex. 12” / 90nm -> 2 Information )
2. Product Size (L*W*H mm)
3. Bumping/Probing site information ( Please provide…
Part Number: LMG708B0 Other Parts Discussed in Thread: LM5137 Hi sir,
Can LMG708B0 do 100% duty cycle for 12Vin/12Vout?
Seems it's okay @ 5V, how about 12V?
If can't 100% duty @ 12V, can it at least +/- 5% full load ?
Like 12Vin to 12Vout ( +…