Hi Joseph,
For clarity, please confirm. You are using the transient PSPICE mode and running time domain simulations (not AC response / Bode analysis).
The TPS7H4001-SP (on the EVM for example) does not require a minimum load for stability at no/low loads…
Part Number: AFE7950EVM Other Parts Discussed in Thread: AFE7950 , AFE7950-SP Tool/software: Hi Team, we are having a requirement of generating/receiving two signals,
1. X Band(around 10GHz)
2. Lower frequency ( < 200MHz)
we want to use single AFE for…
Hi Aurora,
Thank you for sharing the expected delivery date of the EVM. I look forward to the test results!
Additionally, we received feedback from the customer regarding the “load characteristic measurement with reduced input voltage,” and I am sharing…
Dear Evan,
Sorry for the late reply, we were trying some hardware side analysis as a double check
Chris said: Evan Mayhew said: Can you help me understand the purpose of mux on MDIO circuit? We typically do not see switches on MDIO bus.
The MUX is actually…
after disable,Still the same error。
.202784] ------------[ cut here ]------------ [ 1.207519] wiz bus@100000:wiz@5000000: Unable to create SERDES platform device [ 1.215014] WARNING: CPU: 1 PID: 26 at /drivers/phy/ti/phy-j721e-wiz.c:1624 wiz_probe+0xd10…
Part Number: PROCESSOR-SDK-AM335X Tool/software: Hello,
We have a custom board based on am335x EVM. We are evaluating the latest u-boot (20024.04) released as part of the AM335x Dec 2024 SDK. We notice that after issuing a command like "tftp zImage"…
Part Number: J784S4XEVM Other Parts Discussed in Thread: TDA4VH-Q1
Tool/software:
Hello everyone,
We are currently working with SDK 10.0 on a custom board based on the J784S4 and are encountering Linux kernel panics under heavy RAM and CPU usage. This…
Hi kevin,
Thanks for your help. Now I can see 8GB. However, when I try to do memtester, I was able to test 1GB memory but failed if I try 2GB. I attached the log.
Memtester_2GB_Failure.txt
root@j7200-evm:~#
root@j7200-evm:~# memtester 2G
…