Part Number: LMH6321 Other Parts Discussed in Thread: TINA-TI
Hi Team,
Good day. I have a high-speed signal coming to a PCB and I wasn't able to use the high-speed signal (about 20Mhz) directly to the digital input-output card, because of high parsatics…
Part Number: LMH6321 Will connecting the CL pin to GND effectively disable the output current? I would like to use this scheme as a temporary output disable during power-up.
Part Number: LMH6321 Other Parts Discussed in Thread: INA818 , Hi TI Technical Support Team,
I have designed discrete constant current charge discharge circuit. I am adjusting current between 1mA and 10mA using DAC (output voltage corresponding to current…
Part Number: LMH6321
Hi Team, seeking your assistance.
Tried connecting the device using the dual- and single-supply configurations on the datasheet (pgs. 16 and 22), but I ran into overcurrent issues when testing these configurations using an external…
Part Number: LMH6321 Other Parts Discussed in Thread: TL431 , BUF634 Hi, I'm planing to use LMH6321 and would like to use utilizing Vcl pin with setup of 200mA current limit.
But unfortunately I'm not sure how to use Vcl current limit correctly,…
Part Number: LMH6321 Other Parts Discussed in Thread: TINA-TI
Hello Expert,
We are using LMH6321 with a single supply operation. Positive supply V+ for LMH6321 is +15V and Ground pin is at V+/2. With this configuration, there is a 1V of DC shift in the…
Part Number: LMH6321 Hi,
When we connect LMH6321 tab pin to negative rail supply(-15v).it was taking 140mA,and temperature was rising up to 40*C, when tab pin is left unconnected it was taking 30mA only .
Can you please clarify the above issue .
Reg…
Other Parts Discussed in Thread: LMH6321 Has anyone played with the LMH6321 as a HF-range coax cable driver? I'm wondering about its IP2, IP3, NF, etc -- wondering if it'd make a decent "output stage" for low-input-Z loop amps and high-input-Z whip amps…
Part Number: LMH6321 I would like to ask you just in case about the operation of the EF pin.
When Thermal Protection is applied to this pin, the VEF changes as shown in the specifications below. Is there any possibility that the VEF will decrease except…
Part Number: LMH6321 Hi,
When we connect LMH6321 tab pin to negative rail supply(-15v).it was taking 140mA,and temperature was rising up to 40*C, when tab pin is left unconnected it was taking 30mA only .
Can you please clarify the above issue .
Reg…