Part Number: LMH5401 Other Parts Discussed in Thread: BUF802 , LMH6401
Tool/software:
Hi expert,
My customer (Enpower) is evaluating LMH5401 in Osilliscope. They found the output noise is too large (5.8nV/ √Hz ) with below setup, translating to…
Hi Danidu,
What kind of output swing and current drive do you need to achieve from the final stage? For maximum performance I would probably suggest using the LMH5401 FDA followed by LMH6401 VGA as the initial buffer and VGA from the DAC. These parts…
Part Number: LMH5401 Other Parts Discussed in Thread: LMH6401 Hello, experts.
I need the Noise figure vs Gain Settings data for LMH5401.
In case of LMH6401, The data plot supported but LMH5401 doesn't.
LMH5401 Setting is here, TA = 25°C, VS =…
Part Number: LMH6401EVM Other Parts Discussed in Thread: LMH6401 , OPA855DSGEVM , OPA855 Hi there,
I was trying to test the LMH6401EVM output with the square wave input.
As shown in the figure below, the green and purple channels are the differential…
Part Number: ADC12J4000 Other Parts Discussed in Thread: TIDA-00826 , LMH6401 , ADC3662 , On the TIDA-00826 reference design, an LMH6401 is used on an automatic gain control (AGC) loop with ADC ADC12J4000. Why is this block necessary on an oscilloscope…
Part Number: TIDA-00826 Other Parts Discussed in Thread: LMH6401 Hi,
I took the TIDA-00826 as reference and built the simulation by myself as i could not get the complete TINA Simulation file
I am stuck at changing the parameters of the PGA LMH6401…
Part Number: LMH6401EVM Other Parts Discussed in Thread: LMH6401 I have followed installed the 6401EVM software on a desktop PC with the following specifications:
Edition Windows 11 Pro Version 21H2 Installed on 5/20/2022 OS build 22000.832 Experience…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: , LMH6401 We use ADC12DJ3200 to work in JMODE2 mode. The received short transmission test mode data is normal, but when the ADC12DJ3200 normal sampling voltage value is set, the sampling voltage…
Hi Suy,
Yes, that is correct, the 54ohm in parallel times 2, is to make the analog impedance 100ohm differential. No need to consider the capacitive term. Your calculation is correct, 200ohms is ideal for the LMH6401 to drive but 160ohms should be fine…