Part Number: LMH6505 Other Parts Discussed in Thread: LOG300 Tool/software: Currently, we are looking for the replacement of long discontinued Motorola Semiconductor part MC1350D.
This is Monolithic IF Amplifier in SOIC 8 pin.
Let me know the alternate…
Part Number: LMH6505 Other Parts Discussed in Thread: LMH730066 Tool/software: Hi, Team.
We have received the following inquiry from one of our customers:
They were conducting operational checks on the LMH6505 and encountered an issue where the maximum…
Part Number: LMH6505 Other Parts Discussed in Thread: TINA-TI Tool/software: When I simulate a circuit using the LMH6505, I get a 40mV offset at the output. This seems to be independent of gain voltage. My question: Is this real, and is it really independent…
Part Number: LMH6505 Dear support,
I am looking for a variable gain amplifier.
When the input is very high the gain is less, when the input is small, the gain is big.
And the output to be a constant.
Will you be able to recommend to any VGA that…
Part Number: LMH6505 Hi, I'm using this component as a VGA (gain driven by a DAC) and I'm not seeing anything on the output. I'm wondering if I've possibly damaged it.
Configuration: typical application with Rin=10K, Rg=374, Rf=3.74K. Vg limited in…
Part Number: LMH6505 Hi, the LMH6505 in our system runs off of +/5V and has its Vg pin driven by an op amp stage that can swing to the +/-12V rails. There is a 2.7k resistor in series between the op amp and the Vg pin. Fairly often the output of the op…
Part Number: LMH6505 I am working on evaluating the LMH6505 (currently on eval board) as a replacement for the ML1350. I had a quick technical question regarding if the LMH6505 has the possibility of inverting the Gain Control voltage scale. Such as in…
Part Number: LMH6505 Hello,
I am powering an LMH6505 with two LDOs, one which regulates 6V to 5V, and one which regulates -6.5V to -5V. The part is upstream of a differential amplifier that is powered by the same rails. Currently, our power rails are…
Part Number: LMH6505 Other Parts Discussed in Thread: VCA822 , VCA820 , VCA821 , VCA824 , LMH6714 , LMH6609 Hello, My customer would like to use LMH6505 as an AGC described in the figure 49 in the datasheet. However, they would like to use LMH6505 with…
Part Number: LMH6505 Hi
The datasheet of LMH6505 explains that RG determines the input voltage range. I struggle to understand how a resistor which is connected to the output of buffer sets the input voltage range. Can you explain it in further detail…