Part Number: LMH6702 Other Parts Discussed in Thread: DAC5681Z , THS3217 , THS3215 DAC_SCH.pdf
hi,
Please confirm whether above schematic will give output of 0 V to +2.5V. Pin 2 should be connected to neg supply or ground for unipolar positive output…
Part Number: LMH6702 datasheet lists 35°C/W for the 8 lead CDIP package. is this to top case or bottom case? I suspect bottom case, but wish to confirm.
Part Number: LMH6702 Hi Team,
My customer is looking to use LMH6702 with a +7V/-5V as it power supply. Is this ok? I see the maximum power ratings in the datasheet is +/-6.75V. Is this a fixed value relative to GND or is it a voltage rating relevant…
Part Number: LMH6702QML-SP Other Parts Discussed in Thread: LMH6702
Good afternoon,
I am using this amplifier in my front-end circuitry for a lidar system. I am AC coupling to the LMH6702, and supplying a +/- 5V rail. Typically, we are feeding 15nS…
Hi Samantha, keep in mind that a current feedback OPAmp is usually optimized for a certain feedback resistance, which is rather low mostly. The LMH6702 is optimized for a 237R feedback resistance between the output and the -input. When setting a high…
Part Number: LMH6702 Other Parts Discussed in Thread: OPA695 , THS3491 Team,
Looking to see if I can use the LMH6702 to drive a speed pulse (PECL) into a 3-5V 50 ohm load.
I’m not sure I’m in the digital, analog or uwave region.
In the analog…
Part Number: LMH6702 Other Parts Discussed in Thread: TINA-TI How much reverse isolation can this amplifier provide? That is, how much signal is seen at the input in the case where the output is driven. This is assuming a non-inverting gain of 2 circuit…
Other Parts Discussed in Thread: LMH6702 Hi,
we want to use LMH6702 (SOIC) to design a signal generator, how to get the schematic and pcb files of the evaluation boards?
Best regards,
kerb
Other Parts Discussed in Thread: LMH6703 , LMH6702 , LMH6704 Is there any data on output impedance vs frequency for LMH670x?
The datasheets don't seem to have any graphs.
What I'm looking for is a buffer that has low input impedance (<1.6 pF, preferably…