Good evening Vicente, thanks a lot for your answer;
Just for my understanding, what feature in particular makes the LMK00101 preferable to the CDCVF2310?
I see from the datasheet both are 3.3V and LVCMOS compatible, and they have similar prices;
maybe…
Part Number: LMK00101 Other Parts Discussed in Thread: LMK01010 Hi
we need to use the SYNC function of LMK00101. Is this integration way the same as the function of LMK01010?
Can LMK00101 indirectly trigger SYNC function by triggering OE pin to synchronize…
Part Number: LMK00101 Other Parts Discussed in Thread: LMK05318 , I am interested to know if an output from the LMK05318 (OUT7) can be set to HCSL mode and sent to the input of the LMK00101 with DC coupling and 50 ohm external termination on the P and N…
Part Number: LMK00101 Hi,
I'm using LMK00101 in an upcoming project, I'm connecting Vdd to 3.3V, Vddo_Bank_A to 3.3V, and Vddo_Bank_B to 2.5V. having the following requirement for power supply rails: [1] Vdd = 3.3V (24mA); ΔVmax = ±150 mV [2.375V…
Part Number: LMK00101 Other Parts Discussed in Thread: LMK00105 Related to the question in the link: https://e2e.ti.com/support/clock_and_timing/f/48/t/371993?Which-Clock-IC-will-support-TCXO-clipped-sine-wave-input-
I would like to drive the LMK00101…
Part Number: LMK00101 Other Parts Discussed in Thread: LMK00301 , LMK04808 , LMK01010 , LMK01020 Hello,
We are in the process of designing a multi-channel data acquisition system. The ADCs will be spread across several (8 at the moment) daughter boards…
Part Number: LMK00101 Dear Team,
My customer has two questions regarding the LMK00101 I hoped you could help us with :
1. Is it possible to drive the input clock CLKIN0 before the powering of the device? Can it cause damage ?
2. What is the recommended…
Part Number: LMK00101 TI team,
can you please suggest a best way to connect a single ended (3.3V) oscillator to LMK00101. It seems like using the OSCin pin will work best but there is no method describing what is the best practice to do this(and in fact…