Part Number: LMK00308 Hi Experts,
Our customer has a doubt regarding what is the input termination on the clock inputs pins and what should be the trace impedance as he is driving these pins from a clock buffer which is generating a 85ohm HCSL output…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00804 Hi,
We are planning to use this clock buffer LMK00308 to a PLL in our design. Whether the propagation delay and skew will be same for every power ON or changes after next power ON? Kindly…
Part Number: LMK00308 Hello Q1: My customer would like to know the maximum value of JitterADD for HCSL OUTPUT at Vcco=3.3V, RT=50ohms to GND, CLKin=100MHz and Slew rate >= 3Vns. (the datasheet specifies typical value is 77fs) Q2: How much is the…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00304 , LMK1D1204P , In the past, there has been a discussion about where the termination resistor should be placed in relation to LVDS AC coupling.
The link below is a discussion of the location…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00304 , Figure 34 in the datasheet shows how to AC couple the LVDS output when used with a device with internal termination resistors. The issue with this is that the LVDS signal is attenuated by…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00105 Hello team,
I received a question from my customer about maximum power consumption of LMK00308.
In the datasheet, the calculation of power consumption is described in 11.2.
But is there a…
Part Number: LMK00308 Hi Support Team,
Regarding LMK00308, I would like to know the following questions:
About 2 months after start using, one LMK00308's CLKOUTA port clock output stopped. Even if CLKOUTA_TYPE0 is pulled down to GND with 1K ohm, CLKOUTA_TYPE0…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00304 , , LMK00304EVM The output skew specification t_SK(O) for the LMK00308 and LMK00304 is only valid for the same buffer type, e.g. LVDS to LVDS. Do you have any skew data for LVDS out to LVPECL…
Part Number: LMK00308 Hi team,
Could you confirm that CLKout can support DC voltage?
It seems that fCLKin supports DC but I can see no description about CLKout.
Regards,
Noriyuki Takahashi