Hi Jason,
It depends what type of output format you want. I have filtered a list for some of our differential buffer devices with less than 35 ps skew. You can use look into this list to chose for your driver type needs. This list contains new family of…
Part Number: LMK00804B Other Parts Discussed in Thread: CDCUN1208LP , CDCE6214 , CDCE18005 The LMK00804B datasheet says it accepts both single ended and differential inputs.
1) When only using a single ended LVCMOS input, is the output differential?
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Dear experts,
we got a design were a 38.4MHz TCXO with a 0.95V amplitude is AC decoupled connected to "LVCMOS_CLK". Buffer is supplied with 3V3.
Its interesting because at buffer…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hello,
Below is the requirement for our design.
We have a 25MHz crystal oscillator (+/-2ppm) in our design which operates on 3.3V with 0.2V/ns slew rate. We need to generate two clock…
Part Number: LMK00804B Other Parts Discussed in Thread: CDCDB400 , LMK1D1204 Hi
could you help to suggest suitable products to replace SY75572
267MHz 1:2 3.3V HCSL/LVDS Fanout Buffer (microchip.com)
Part Number: LMK00804B Hello, What is the maximum IDDO,Cload that LMK00804B can sink/source per one output? Or what is the maximum Cload that LMK00804B can drive per one output? Best regards, K.Hirano
Part Number: LMK00804B-Q1 Hi Team,
Are the VDDO Output Supply terminals 11 and 15 tied together on the die or do they supply two separate outputs each?
Thank you
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804 Hi, Good day. Our customer would like to know if there's a published specification for the output (Q0 - Q3) drive current capability of this device?
It is able to drive the standard…
Part Number: LMK00804B-Q1 Hello Team,
What is the Absolute Maximum Rating for Continuous Output Current (Io) that is not listed on the Datasheet?
Regards,
Renan