Part Number: LMK01000 Simon, thank you very much for your help.
Well, this is just actual measurement data, and you don't have MIN and MAX spec at this time, correct ?
Part Number: LMK01000 Hi TI,
I'm sorry but my custoer still need the Tr/Tf of LVPECL output spec( or Actual data).
The frequency are 148.5MHz and 297MHz.
Part Number: LMK01000 Other Parts Discussed in Thread: LMK03000 , Team,
Can you please specify the minimum swing for differential outputs on the LVDS and LVPECL pin pairs when Vboost is set to 1. Only the nominal is specified.
Your support would be greatly…
Part Number: LMK01000 Hi,TI,
I cannot find the Tr/Tf sepc of LVPECL output.
Please let me know the Tr/Tf spec or actual result ?
A clock receiver device required TrTf ≦ 500ps(800mVpp MAX).
Hi Kadeem,
So we replaced the 2nd stage LMK03033s with LMK01000 and that looks good: inputs and outputs are in phase and the timing for the ADC is about the same for ADCs clocked by the same LMK01000 or different LMK01000s (about 120 ps each case)
The…
Other Parts Discussed in Thread: LMK01000LMK01000 output skew is typically 4 ps and no more than 30 ps,For a particular chip, the channel skew is a fixed value or a random value?Skew between the channels will change after each re power up?
I'm planning…
Other Parts Discussed in Thread: LMK01020 , LMK01000 Hi,
I'm using lmk01020 for distributing 550 MHz and its div2 for using 3 samples of each frequencies. My question is about additive jitter due to using divider relative to only distribution path and of…
Other Parts Discussed in Thread: LMK04828 , LMK01000 Hi,
Comparing two clock buffer parts(using PLL section is not my plan), LMK01000 & LMK04828 is my question. The additive jitter performance of lmk01000 part is excellent in class(in 100 to 20 MHz SSB…
Hello Libby,
To directly answer your question, the LMK01000 won't work for your application because it does not have a divider value at any output that will result in 200 MHz from a 1GHz signal. You need a divider value = 5 and the LMK01000 divider values…
Q1: What is the approximate differential input impedance for the CLK0 and CLK1 inputs?
Q2: In the Electrical Characteristics table is the input clock power specification (Pclkin) range given differential input power or power per input pin as implied by…