Part Number: LMK01020 Hello,
LMK01020's data sheet only specifies Θ JA and Θ J-PAD (Thermal Pad) as thermal parameters of the LMK01020, but I don't think that's enough. Could you also provide such thermal parameters as Θ JC …
Hi Shinichi,
I apologize for getting back late in this. I was trying to get more information from packaging team. It seems that we don’t have this data for this package. Heat sink should be okay to use but we don’t have specific number. This…
Hi Jose,
Do you think we could change this setup to a more simple solution by using LMK01020 (first stage) with /4 to get the 25MHz clock and then using a 2:8 LVPECL buffer CDCLVP1208 (second stage) on the first stage outputs ? Since skew in second stage…
Part Number: LMK01020 Hello,
My question is what options / how to properly terminate the unused differential clock inputs of the LMK01020.
In our design, we use several LMK01020 devices,
The master LMK01020 uses both CLKIN0 and CLKIN1 differential inputs…
Part Number: LMK01020 Hello team,
I would like to know Output duty information of LMK01020 but there is no spec/description about output duty in its datasheet.
Could you let me know output duty of LMK01020?
If it changes depending on divider ratio, please…
Part Number: LMK01020 Hi Team, Posting for our customer. Do we have a characterization on the typical propagation delay of LMK01020 between its input (CLKin) to any of the outputs (CLKout) straight through (No divider, No fine delays)? Thanks in advance…
Part Number: LMK01020 Hi, we are using the LMK01020 device in our design for providing LVPECL clocks to ADCs. I would like to get the design reviewed before releasing Gerber files.
Attaching the schematics of the LMK01020 section. B100_0.94V_For_Review_TI_LMK01020ISQE…
Part Number: LMK01020 Other Parts Discussed in Thread: CDCLVP1204 , LMK03806 , CDCM6208 Hi,
I have a application:the input is 600MHz single ended signal, Output is differential signal.
I want to know what is the maximum input frequency(single ended)…
Part Number: LMK01020 I need help on 2 questions w.r.t. LMK01020.
1)Unused Clock outputs termination:
out of 7 LVPECL output clocks i am using 5, 2 will be unused in my design so in that case should i terminate the unused clocks or can i just leave…
Part Number: LMK01020 Other Parts Discussed in Thread: LMK04828 Hi E2E,
Good day!
I have a customer that is having a register value mismatch (comparing to datasheet). The mismatch is on registers R2 to R7 bits A3-A0. From what I know, these bits are…