Part Number: LMK03328 Other Parts Discussed in Thread: , LMK04832 Hi,
In my application, I have a clock of around 70MHz. This clock has significant jitter. I need to double this clock and filter the jitter as much as possible.
I am struggling, however…
Part Number: LMK03328 Other Parts Discussed in Thread: USB2ANY , Hi,
In my application, I have 2 input clocks, only one of which is active at any given time, and 2 different output clocks which are always active.
I need to switch between input clocks…
Part Number: LMK03328 I have a question about I2C access failures. In another thread, we found an I2C access failure event with a frequency of 1/1000.
LMK03328: POR spec - Clock & timing forum - Clock & timing - TI E2E support forums
We too have…
Part Number: LMK03328 Hi Team
I have downloaded IBIS model form website , for using with Hyperlynx but only 1.8 V output models are available . If same model is applicable for 3.3V ? If not how i can simulate for 3.3V ?
Part Number: LMK03328 Hi Team We are using LMK03328 LVPECL output in one of our appliaction for generating various various reference clock for differrent PHY . Below are the spec of REFCLK
1) Vppd=600-1200 mV Rdiff=80-120 ohm , Internally biased , internal…
Part Number: LMK03328 I have a question when programming the LMK03328 device.
I am generating the register set via TICS Pro (v1.7.5.15). I am programming the device in soft pin mode exclusively using I2C transactions. I am trying to integrate these values…
Part Number: LMK03328 I am in the process of verifying the operation of an LMK03328 Clock device where is it relying on the secondary input input clock that is being used to drive PLL2. I want to verify that the PLL2 is locked by reading registers on…
Part Number: LMK03328 Hello expert,
My customer is using LMK03328 in their project. They would like to know if I2C frequency measured 52kHz is normal or not. Since the spec is within 100kHz to 400kHz, 52kHz is out of this spec. Thanks a lot!
Best regards…