Hi Jaime Martin,
Here is a better comparison. The reference is a 100 MHz WENZEL
But to your point, you are absolutely correct. If you are driving LMK04805 PLL1 configured for relatively low bandwidth, the broadband noise floor is irrelevant. Either buffer…
Hi again. I am now changing from the 04906 to the 04805. I think i don't have to worry of the fact that the output frequency spec for th former is 2.6GHz while the one for the latter is 1.536Ghz, as far as the outputs are really exactly the same type…
Other Parts Discussed in Thread: LMK04805 Hi,
I'm trying to use the LMK04805B for a new design with the following configuration:
- Single PLL (PLL2), internal VCO, 0-delay mode,
- Oscin = 38.5MHz
- CLKout0 = 154MHz (NO_SYNC_CLKout0_1 activated because…
Other Parts Discussed in Thread: LMK04808 , CDCE62005 , LMK04805 Customer want to know the LMK04808 channel isolation. such as output frequency on channle 0, how many dBc you can measured on channel 1?
this parameter can be find on CDCE62005 datasheet page…