Hello Nir,
Nir Flysher said: What will be the right TSW platform to demo the DAC3482EVM ?
You can use the TSW1400 platform, which provides LVDS data stream to the DAC3482 EVM
Nir Flysher said: Customer wanted to highlight multiple mistakes found on the…
Part Number: LMK04808 Other Parts Discussed in Thread: LMK04832 We need a JESD204B clock device who can export clock as 2880MHz or 3000MHz.,like LMK04808.But the datasheet say:Clock Rates of up to 1536 MHz,so,can we use LMK04808?
Part Number: LMK04808 Hi team,
My customer use the LMK04808 and all the register setting is OK.
Now there is a new application that they need to use the software to reconfigure the R27 register as the same value.
So the process is as below:
1. Initialize…
Part Number: LMK04808 Tool/software: WEBENCH® Design Tools Hi TI experts,
LMK04808B has two PLLs. The VCO of PLL1 is an external VCXO or a tunable Crystal.
However, the entry to specify the frequency of VCXO is not found the WeBench Clock Architect design…
Part Number: LMK04808 Other Parts Discussed in Thread: TPS7A7300 Hi team
My client configured the system with the following blocks.
LMK04808 does not work properly when testing -5 ° operation to chamber.
Normally, PLL2 should operate in cascade after…
Part Number: LMK04808BEVAL Other Parts Discussed in Thread: LMK04808 Hi Team,
Customer is testing the LMK04808 EVM and wants to determine whether clkin0 is present. However, the status level of clkin0 does not change when there is no reference.
Could you…
Part Number: LMK04821 Other Parts Discussed in Thread: LMK04808 Hi Dear experts,
My customer recently changes VCXO supplier, the VCXO output impedance is different from previous supplier. They want to know what is LMK04821/LMK04808 OScin pin input impedance…
Part Number: LMK04808 Other Parts Discussed in Thread: CODELOADER hi team,
we meet LMK04808 periodic unlock problem, it`s unlock every 5~10 minute, the SCH is the same with EVM, and configuration is as below:
is there any configuration problem?
or do…