Part Number: LMK04816 Other Parts Discussed in Thread: ADS5400 , DAC5682Z , , LMK04828
Hi Team,
I develop board with 10 x DAC5682Z & 2 x ADS5400.
I looking for clocking solution, I saw LMK04816/28 but it will be great if you can suggest your recommendation…
Part Number: LMK04816 I tried the following methods: 1. Use power divider to connect input clock to CLKin1 (FBCLKin) and CLKin0. Use 0 delay mode, and choose FBCLKin as feed back. The result is that the output clock can be synchronized with the input clock…
Hello,
(1) Understood.
(2) The answer is insufficient.
2-1 Is "10ns" the setup time, the hold time, or both?
2-2 Which signal is "10ns" relative to? Please tell me the reference signal.
2-3 Please tell me the assertion time of the…
Part Number: LMK04816BEVAL Other Parts Discussed in Thread: LMK04816 I have a LMK04816 Eval board from which I am trying to get 125 MHz and 6.25 MHz clock signals. I have a 50 MHz clock signal that I can bring onto the board. The board is equipped with…
Part Number: LMK04816BEVAL Other Parts Discussed in Thread: USB2ANY , LMK04208 , LMK04816 , CODELOADER , USB2ANY-UWIRE I cannot program my LMK04816B Eval board. I am trying to do the quick start scenario in the manual using a USB2ANY adapter.
I have replicated…
Part Number: LMK04816 The board designed by ourselves, the same output circuit design and the same LDO provide 3.3V power supply for vcc_clkout.
Using software to configure the same frequency output frequency (2.4 GHz) and the same level standard (LVPECL…
Part Number: LMK04816 Other Parts Discussed in Thread: CODELOADER Hi All.
I'm using the LMX04816 Eval Board with PC -- LPT-uWire cable.
When I try to select in 'Select Device' LMX04816 CodeLoader display Run-time error '13' and shut down.…
Part Number: LMK04816 Hi,
Regarding the programming of 32 registers of LMK04816, is it performed after each register is written or after all registers are written?
If two outputs are placed in two different GROUP (switch bits in different registers)…
Part Number: LMK04816 Hi,
Regarding the programming of 32 registers of LMK04816, is it performed after each register is written or after all registers are written?
If two outputs are placed in two different GROUP (switch bits in different registers)…
Part Number: LMK04816 Hello,
I need to simulate and calculate phase noise of LMK04816 in the 0-Delay Dual PLL , using Clock Design Tool . I don't find the way to configurate this software to implement the configuration.
Note: This configurations has…