Part Number: LMK04832 Other Parts Discussed in Thread: DS250DF410 Tool/software: I'm trying to use the LMK04832 to generate a 1.611328125GHz Clock.
I'm targeting using LVPECL 1600 Format at the Output of the LMK04832.
The 1.611328125GHz Clock {LMK…
Part Number: LMK04832 Tool/software: Hi,
I would like to synchronize the pulse input from Clockin0 with Clockin1 (312.5MHz) on the LMK04832 and output it from Clockout9, 11, and 13.
It seems that the block diagram in TICS.Pro is set up correctly,…
Part Number: LMK04832 on your datasheet for LMK04832 - there are 2 footprints for the Device NKD0064A and NKD0064B
which device is the correct one to use?
LMK04832 Ultra Low-Noise JESD204B Compliant Clock Jitter Cleaner With Dual Loop PLLs datasheet…
Part Number: LMK04832 Hello,
I’m working for Thales in PCBA Department as process technologies engineer. I need to get the die dimension (length and width) of the component "LMK04832NK" to validate the use for our products. This information is not available…
Part Number: LMK04832 Tool/software: Hi,
This is Dinesh from iWave Global. I have a doubt regarding the use of LMK04832 clock file in LMK04368 Clock Synthesizer. Please confirm this if we can use.
If I provide 3000MHz in VCO1, the PLL2 is not locked…
Part Number: LMK04832 Tool/software: Hi,TI Team:
I would like to know the detailed locking process of PLL1/2 in Nested 0-Delay Dual Loop Mode.
How long does it take for PLL1/2 to lock (the loop filter bandwidth is shown in the figure)?
During the…
Part Number: LMK04832-SEP Other Parts Discussed in Thread: LMK04832EVM Tool/software: Hi,
This is Dinesh from iWave Global. I need to clarify the Supply Voltage for LMK04832-SEP. In the datasheet, it is mentioned as VDD and VDD_A as 3.3V but in the…
Part Number: LMK04832-SP Tool/software: Dear team,
Kindly confirm the maximum output frequency which we can generate continuously using the LMK04832-SP.
Part Number: LMK04832 The LMK04832 datasheet contains information on two different packages (NKD0064B, NKD0064A).
I cannot identify which of these packages it is from the part number.
I will use the LMK04832NKD.
Which package dimensions should I…
Part Number: LMK04832 Tool/software: I'm using the LMK04832 in Dual Loop Mode.
1. PLL1 Reference is 100MHz
2. PLL2 Reference is 156.25MHz External VCXO [Fed into OSCin]
3. PLL1 R = 16, PLL1 N = 25
4. Goal is run PLL2's Internal VCO [VCO1] @…