Hello Hirotaka,
Yes, it is possible to place the LMK05318 B on the LMK05318EVM. You will have to de-solder the LMK05318 currently on the board and then solder on the LMK05318 B .
Regards,
Kia Rahbar
Part Number: LMK05318B Other Parts Discussed in Thread: LMK05318 , , CDCE6214 Hi, I have some question for LMK05318 as below:
1. Can the 180.25Mhz used for 15" screen refer to XO output as shown below, and the 24.576Mhz used for audio refer to PRIREF output…
Part Number: LMK05318 Hi this is my first time using the LMK05318. Under normal operation in free air what kind of temperature rise would be expected. From the datasheet I'm seeing core is typically around 0.75W so even rounding up to 1W to allow margin…
Part Number: LMK05318 Other Parts Discussed in Thread: TICSPRO-SW Hi all Would you mind if we ask LMK05318? We would like to confirm Digital Loop filter setting like as follows; By setting of DPLL's loop band with run script operation on TICSPRO-SW, does…
Part Number: LMK05318 Hi team,
Could you help share how could we disable all the output using hardware? Only pull low PDN could do this?
If using software, how should we do this?
Best Regards,
Will
Part Number: LMK05318 Other Parts Discussed in Thread: LMK5B12204 Hi Team,
Do we have any chips need support 4 channels output at the accuracy of LMK05318? Can you recommend the suitable one?
Best Regards,
Gust
Part Number: TICSPRO-SW Other Parts Discussed in Thread: LMK05318 Hi all Would you mind if we ask TICSPRO-SW using LMK05318? Our customer doesn't use SEC_REF, they use only PRI_REF. In this case of SEC_REF=0, with Run Script, there is the error message…
Part Number: LMK05318 Other Parts Discussed in Thread: LMK03328 Hi all Would you mind if we ask LMK05318?
Our customer would like to confirm DPLL lock and valid of reference. We assume that following methods are valiable. 1. Check of PRIREF_VALSTAT using…
Part Number: LMK05318 Hi team,
Customer is designing LMK05318, they get two questions related with XO clock input:
1. What's the swing spec if XO is AC coupled single end input as the datasheet shows? I see datasheet shows DC coupled, differential input…