Part Number: LMK1C1102 Hello SIr,
The datasheet of the LMK1C1102PWR mentioned the output needs 5 cycles CLKin,
but in our application, the output enabled only used one cycle (as below waveform).
Since currently we're adjusting the FW behavior, we need…
Part Number: LMK1C1102 Does the 1G output enable disable the output buffer to allow 2 different LMK1C1102 devices to drive the same signal - as in the pic below? Is it a Hi-Z output when disabled or driven low? I'm trying to select between 2 different…
Part Number: LMK1C1102 Hello expert,
My customer would like to know if LMK1C1102 CLKIN pin can be placed floating or not. Could you kindly answer for it?
Based on datasheet table 9-1, it seems like CLKIN could be floating but the output will be pulled…
Part Number: LMK1C1102 Other Parts Discussed in Thread: LMK00804 , LMK00105 Hi Experts
does LMK1C1102 p2p 83026BGI-01LFT?
I check it on datasheet
they both are TSSOP package . but they don't have same pin position.
could you help me double…
Part Number: LMK1C1102 Hi,
In the datasheet it is stated that the output impedance is 50 ohm, but in the application example (section 10.2) it is sugested to use a serie resistor even though the transmission line is 50 ohm.
What is the explanation for…
Part Number: LMK1C1102 t1G_ON and t1G_OFF are specified as maximum cycles (5), with no minimum. Are there conditions where this is the guaranteed minimum as well? i.e., setup time, hold time, specific frequencies?
I would like to use this part as part…
Part Number: LMK1C1102 The datasheet has the plot below., but I am interested in the actual 1/f corner and absolute noise floor for the part. Do you have a plot when driven by a high quality Wenzel OCXO at 100MHz?